Boards for XIAO Camera

Is there a board other than the XIAO ESP32-S3 Sense, where I can plug a XIAO camera (the same one that is used in Sense)? I have an extra camera. I am looking for another board to use this camera (e.g. B2B connector?). Thanks.

Regards.

Hi there,

So , for some reason I’m thinking it works with the Grove Vision AI2 ?
Very cool product as well. :+1:

HTH
GL :slight_smile: PJ :v:

… but the Grove Vision AI (under the belt too,:grinning_face: ) has a camera already. Thx.

Regards.

It looks like there is no other option but to keep the extra camera as a spare part.

You can use one of these;

SD card holder for MMC mode on the back.

There are also converter boards that have a camera connector on them with the pins then available on a couple of rows of 0.1” pins, look for FPC FFC adapter boards.