Blurred lines with new camera on XIAO ESP32-S3-Sense

The title says it all. i just changed the base camera coming with the XIAO ESP32-S3-Sense for this : OV5640 Camera for XIAO ESP32S3 Sense (With Heat Sink) - from QVGA(320*240) up to QSXGA(2592*1944), 8/10-bit RGB RAW Output, auto-focusing - seeed studio and without changing anything with the example code i now see lines in the image.

im wondering if i have to change things in the example paramaters. I first looked at the connection and it doesnt seems to have much room for misalignement so i guess its a software problem.

Any ideas ?

Id like to know if can upgrade quality with this new cameraas well. i dont see much improvement…

thank you guys !

Hi there,

I would say it’s a settings thing.
You on the camera web server page ? ,you can adjust the parts for that camera.
:smiling_face_with_sunglasses::+1:

Check the WIKI… For the S3 sense version

HTH
GL :grin: PJ :victory_hand:

nop, i dont use the server. id like to be able to tune it in software, how can i do it ?

Hi there,

So, It’s been a minute on using it, you create a .json file in the server app that you can use as the config AFAIK. You need to look at the camera wiki, & GIT they are adding stuff Quarterly on some of those products.

HTH
GL :slight_smile: PJ :v: