Hello everyone,
Does anyone have the Bluetooth Multimeter working?
Has anyone managed to download the software without problems? I can’t unzip without errors on any of files.
Is the meter already pre-programmed with the software? Or do I need to use the Arduino IDE, of which I don’t have a clue how to use!
I have used the UartSBee connected to PC via a USB cable, should I see any information from the meter? I get an intial character (looks like it could be ‘BT’ icon) response but then nothing else.[size=1]reverse image search email checker port checker[/size]
Can anyone help?
Seemed like a good idea at the time! 
Hi @reddingtonisasgoodasdembe,
Could you please share more details like Which model multimeter are you using and what was the error .