Industrial Box PCs reComputer Industrial J3011- Fanless Edge AI Device with Jetson Orin Nano 8GB module, Aluminum case with passive cooling, 2xRJ45 GbE, 1xRS232/RS-422/RS-485, 4xDI/DO, 1xCAN, 3xUSB3.2, Pre-installed JetPack System
This one, SO For the Seeed Studio reComputer Industrial J3011 (Part Number 110110193), adding Bluetooth functionality requires using an M.2 Key E wireless module. Because the Jetson Orin Nano module itself does not integrate onboard wireless, connectivity is expanded via the carrier board’s standard M.2 Key E slot.
Supported Modules & Hardware Requirements
Recommended Modules: Standard M.2 Key E Wi-Fi/Bluetooth combo cards natively supported by the Linux kernel and NVIDIA JetPack work best. Commonly deployed options include:
Intel AX210 / Intel AX200 (Wi-Fi 6/6E + Bluetooth 5.2/5.3) — widely used and well-supported out-of-the-box by Ubuntu/JetPack kernel drivers.
Realtek-based M.2 Key E cards (such as the RTL8822CE or RTL8852BE), which Seeed frequently utilizes across their Jetson ecosystem.
Antennas & Accessories: You will need an M.2 Key E card that includes or is paired with IPEX/MHF4 to SMA antenna cables and external antennas. Because the industrial aluminum enclosure provides heavy RF shielding, the antennas must be routed through the enclosure’s designated antenna knockouts/ports to maintain a reliable Bluetooth and Wi-Fi link.
Software & Drivers
Drivers: Most standard Intel and Realtek cards have open-source drivers included in modern Ubuntu/Linux kernels. Depending on the exact JetPack version pre-installed on the unit, firmware packages (linux-firmware) may need to be updated via apt to ensure the Bluetooth HCI controller initializes properly.
Configuration: Once physical installation is complete, Bluetooth can be managed directly via standard Linux utilities (bluetoothctl or standard desktop network settings if a GUI environment is active).