Blink sketch compiles, but here is what I see when I upload it to the Seeeduino v4.2 board.
Arduino: 1.8.3 (Windows 7), Board: “Seeeduino V4(Atmega328P)”
Sketch uses 1030 bytes (3%) of program storage space. Maximum is 32256 bytes.
Global variables use 9 bytes (0%) of dynamic memory, leaving 2039 bytes for local variables. Maximum is 2048 bytes.
java.io.IOException: Cannot run program “REMOVE/bin/avrdude”: CreateProcess error=2, The system cannot find the file specified
at java.lang.ProcessBuilder.start(ProcessBuilder.java:1048)
at processing.app.helpers.ProcessUtils.exec(ProcessUtils.java:26)
at cc.arduino.packages.Uploader.executeUploadCommand(Uploader.java:129)
at cc.arduino.packages.uploaders.SerialUploader.uploadUsingPreferences(SerialUploader.java:207)
at cc.arduino.UploaderUtils.upload(UploaderUtils.java:78)
at processing.app.SketchController.upload(SketchController.java:713)
at processing.app.SketchController.exportApplet(SketchController.java:686)
at processing.app.Editor$DefaultExportHandler.run(Editor.java:2149)
at java.lang.Thread.run(Thread.java:745)
Caused by: java.io.IOException: CreateProcess error=2, The system cannot find the file specified
at java.lang.ProcessImpl.create(Native Method)
at java.lang.ProcessImpl.(ProcessImpl.java:386)
at java.lang.ProcessImpl.start(ProcessImpl.java:137)
at java.lang.ProcessBuilder.start(ProcessBuilder.java:1029)
… 8 more
An error occurred while uploading the sketch
This report would have more information with
“Show verbose output during compilation”
option enabled in File -> Preferences.
Thanks,
Steve
Now it is working with Seeeduino V4(ATMega328P) and Arduino / Genuino Uno board setting.
Thank you!
Steve