… And… initial attempt, using a Linux machine (UBUNTU 16.04/AMD 64X2/8GB Mem), FAILED… no change, it still had the blank-white screen…
However… I think I went to the MIN main forum, and located a post, that had two .hex files, claiming to be the original firmware… tried it via the same Linux machine… FAILED…
Now, this is where my old Hardware addiction pays off…
A friend was downsizing their equipment, and asked me if I wanted their old machine… Core2-Duo, 4GB mem, Windows Vista (X32), dug around, and managed to find a copy of the DFusr-Demo, Nahhh… Couldn’t be that easy?
loaded it… Plugged the scope into the USB port, It accepted the DFU drive… copied the two hex files again… it dropped connection after the files transferred, then reconnected… this time, both .hex files were replaced by “.RDY”. Okay, turned off the scope, and turned it back on… This time, instead of the short MIN label screen, and then solid white, I got the short label screen, followed by Bright/Dim flashing back & forth. found the file you linked… copied it… thisw time, came up “.ERR”… found the3 copy of the old original files I had… showed “.RDY”… cycled the scope, and… Slow as molasses, But it was Working! grabbed the 3.64 BenF firmware. “.RDY” and WORKING!!! DeBricked!!