Hi All,
Looking at the schematic for BGW, I can see that there are can be 2 antennas in parallel…
1 chip antenna (on-board) and 1 external antenna.
(And there is no option to switch between chip antenna and external antenna, as it is hard wired).
Will the wifi performance be ok with 2 antennas on 1 output of WL1835??
2G4_ANT1_WB connect to 2 antennas (chip ant1 and J6 external)
Thanks,
Martin L.