Hello all,
I have a new BBGW and have updated it to the latest Debian (4.14.108-ti-r104).
I want to do audio I/O using a C-Media sound card. 
The lsusb command tells me,
Bus 001 Device 003: ID 0d8c:0102 C-Media Electronics, Inc. CM106 Like Sound Device
and aplay -L appears to find the card’s many ports (including surround-sound), but any attempt to actually play or record results in responses like,
aplay -D front Flute02.wav
ALSA lib confmisc.c:767:(parse_card) cannot find card ‘1’
ALSA lib conf.c:4528:(_snd_config_evaluate) function snd_func_card_driver returned error: No such file or directory
ALSA lib confmisc.c:392:(snd_func_concat) error evaluating strings
ALSA lib conf.c:4528:(_snd_config_evaluate) function snd_func_concat returned error: No such file or directory
ALSA lib confmisc.c:1246:(snd_func_refer) error evaluating name
ALSA lib conf.c:4528:(_snd_config_evaluate) function snd_func_refer returned error: No such file or directory
ALSA lib conf.c:5007:(snd_config_expand) Evaluate error: No such file or directory
ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM front
aplay: main:788: audio open error: No such file or directory
I’ve found a load of conflicting and stale web pages about editing the various boot-time, ALSA-config and lodable-driver files.
It looks like ALSA is in transition; several of the packages have been recently removed.
Does anyone have experience using a generic USB sound card on a BBGW?
(It’s been quite a while since I’ve hacked drivers.)
…any reply appreciated…
stp in SB CA
To add some more detail, if I try the simplest aplay command,
 aplay Flute02.wav
I get the error message,
ALSA lib dlmisc.c:254:(snd1_dlobj_cache_get) Cannot open shared library /usr/lib/arm-linux-gnueabihf/alsa-lib/libasound_module_pcm_front.so
aplay: main:788: audio open error: No such device or address
but there isn’t a directory named /usr/lib/arm-linux-gnueabihf/alsa-lib and the closest related-looking library is,
/usr/lib/arm-linux-gnueabihf/libasound.so.2.0.0
This looks like a link-time problem that doesn’t match the installed libraries.
I updated the alsa and libasound packages using apt-get.
Do I need to recompile and link this?
Is there a collection of the ALSA config files that works with BBGW and USB sound cards?
…any assistance greatly appreciated…
stp in SB CA
Hi there, 
I used the respeaker mic array v2.0(UAC 1.0) and it works well with the bbgw. thanks. 
http://wiki.seeedstudio.com/ReSpeaker_Mic_Array_v2.0/
</s>debian@beaglebone:~$ uname -a
Linux beaglebone 4.14.71-ti-r80 #1 SMP PREEMPT Fri Oct 5 23:50:11 UTC 2018 armv7l GNU/Linux
debian@beaglebone:~$ aplay -l
**** List of PLAYBACK Hardware Devices ****
card 1: ArrayUAC10 [ReSpeaker 4 Mic Array (UAC1.0)], device 0: USB Audio [USB Audio]
  Subdevices: 1/1
  Subdevice #0: subdevice #0
debian@beaglebone:~$ arecord -l
**** List of CAPTURE Hardware Devices ****
card 1: ArrayUAC10 [ReSpeaker 4 Mic Array (UAC1.0)], device 0: USB Audio [USB Audio]
  Subdevices: 1/1
  Subdevice #0: subdevice #0
debian@beaglebone:~$ arecord -D plughw:1,0 -f cd test.wav
Recording WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
^CAborted by signal Interrupt...
arecord: pcm_read:2103: read error: Interrupted system call
debian@beaglebone:~$ aplay -D plughw:1,0 -f cd test.wav
Playing WAVE 'test.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
debian@beaglebone:~$<e>
Thanks for your response!
After reading a lot and editing the config files (/etc/modprobe.d/alsa-base.conf, /usr/share/alsa/alsa.conf, /etc/asound.conf), I got it working with the c-media usb sound card. 
The only issue is that for some reason, I have to sudo the alsa commands for them to work.
I log in as user “stp” and here’s what it looks like:
_ stp@~ _ uname -a
Linux RoCoCo_0 4.14.108-ti-r104 #1 SMP PREEMPT Tue Apr 9 18:16:29 UTC 2019 armv7l GNU/Linux
_ stp@~ _ aplay -l
aplay: device_list:270: no soundcards found…
_ stp@~ _ sudo aplay -l
**** List of PLAYBACK Hardware Devices ****
card 1: Device [USB Sound Device], device 0: USB Audio [USB Audio]
Subdevices: 1/1
Subdevice #0: subdevice #0
I added stp to the audio group in /etc/group.
I can’t figure out why this is necessary, but I can work with it…
stp
Hello bill,
So you installed this library https://github.com/respeaker/usb_4_mic_array on the beagle bone and the respeaker operated right ? while connecting the mic to the usb host.
Or are there any extra steps needed to operate on the beagle bone ? and is it the same for either black, green or the green wireless?
Thanks s lot.