Battery voltage monitor and AD conversion for XIAO_ESP32C

@msfujino
It’s quite old thread, but could you help me to understand the reasoning behind the selection of resistors?
You use 220 kOhm resistors, which gives me 8 microA.
The other guy here in the thread suggests to use 1MOhm resistors, which gives 1.85 microA.
I believe both options work for you guys, I’m just not sure why would I choose one over another. Which are min and max current limits?
Thanks for the help!