Barometer readings incorrect after sleep

Hi Wio team, I’ve encountered a problem with the BMP180 Barometer grove. I can make it work on the Wio using the BMP085 firmware, but when the Wio wakes after a sleep, the values from the barometer are completely random. Any suggestions on how to fix this? Is there some way I can “reset” the barometer in the ULB or via a REST request? Thanks in advance!