Hi, I’m having an issue with the Barometer module, where in when my project is powered up, the Barometer and Temperature values report by the sensor are all over the place. The odd thing is if I touch the Oscillator on the module, the values immediately stabilise and are correct from then on.
Rather than repeat myself, the full details are on this thread on the GHI forum, which is where I brought the 3 modules I’m having issues with.
tinyclr.com/forum/topic?id=7 … 3#msg78240
Any advice would be appreciated!
Thanks,
Stephen.