I’ve just got this clock but I fail to set the time. No matter where and how I tap it, it doesn’t enter the mode to set the time. The manual says open the clock & turn it on by pressing the button, then tap it twice on the front. Tried that several times, it doesn’t work. Is there a way I can check the gyro sensor?
There isn’t a gyro sensor include this kit .
It would be work if the hardware connection is right , please check it again refer to the documentation .After make sure the connection is right , you can try to test if Chip mega328 can work right with a Arduino Uno . If so , then re - upload the firmware to mega328 , you can find the firmware at http://wiki.evilmadscience.com/Bulbdial
Any more question , please email to me [email protected]