AWS SEEED IoT 1-Click Button not registering with WiFi via iOS app

Seeing the same thing. Just bought the SEEED IOT BUTTON FOR AWS and downloaded the AWS IoT 1-Click app (v1.4.4.0). After providing my Wi-Fi information, the screen gets stuck at “Configuration: In progress”. The button showed up briefly at one point in Bluetooth; but it doesn’t seem to ever show up again. The Blue LED (which was blinking) eventually seems to time out and just stops flashing. Would really like to get this all working. Maybe I’ll try a different phone and my iPad…but not having much success at this point.

Update: So, I can put the button into Bluetooth mode and my Laptop (Windows 10) can see it and I can add it as a device. However, I’m not seeing that button communicate with either of my iPhones (I have an 11 and an 8 Plus…both on the latest Apple iOS). Will continue to plow ahead and see if I can get this thing to work.