What is the best Programmer board for experimenting with ATTiny chips
https://www.amazon.com/KOOBOOK-USBtinyISP-Programmer-Bootloader-Interface/dp/B07S9BX98K
https://www.amazon.com/naughtystarts-Development-Programming-Replacement-Compatible/dp/B0B18P2CBJ
I am looking at the small ATTiny, but would like to get something that can program the larger sized ones if i need more GIPO
any experience?
check this out,
which TINY ? grab this and put it on the Arduino you already have and go to town.
IMO , you can’t beat a Tiny85 anything bigger is better on arduino,
84 if you want more pins.
Use the AtTinyCore LIB on Arduino IDE and this link:
ATtiny 25/45/85
HTH
GL
PJ 
fyi , read the GitHub link and there are a million usb Programmer Clones out there. .
nice good links i will check out
That is actually the one i want, but it is an old kickstarter… the kid is probably on mars by now
I am working on the “Project” conceptual
I need a device to drive 3-6 led, i read about pin multiplexing but that will cause flicker and it is important to my project for all leds to latch at the same time, i want to communicate with the control chip by IIC,
and the sensor chip is already IIC but fixed address, so i will have to either connect it to the AT to translate or set up a separate multiplexer bus
so i think
a 14 pin would do it, or 2 x 8 pin would do same…