AT+ --> +ERR=-3 on a freshly bought board

Hello,

Only now I bought two boards on Aliexpress. I took it out of the package and checked it strictly following the instructions(Wiki getting started).

Unfortunately I can not get an answer OK.



At first I used SSCOM as stated on the wiki, but without success.

After that, I connected the boards to Raspberry Pi and just sent the lines to the preconfigured(115200 8n1) /dev/ttyUSB0 device.

====

rabbit@raspberrypi:~ $ echo -ne ‘at+\r\n’ >/dev/ttyUSB0

rabbit@raspberrypi:~ $ echo -ne ‘at+\n’ >/dev/ttyUSB0

rabbit@raspberrypi:~ $ echo -ne ‘AT+\r’ >/dev/ttyUSB0

====

other console:

====

+ERR=-3+ERR=-3+ERR=-3

====



Tell me, please, what else can I do to make these things to work?

Some pictures. The modules were in sealed bags, there was silica gel as well. I just pulled them out and tried to execute the simplest AT command.
[attachment=3]test.png[/attachment]
[attachment=0]IMG_20190613_081810_HDR-min.jpg[/attachment]
[attachment=1]IMG_20190613_082536_HDR-min.jpg[/attachment]
[attachment=2]IMG_20190613_082646_HDR-min.jpg[/attachment]




As it turned out, it doesn’t understand 'AT’or ‘AT+’, but it responds to ‘AT+GMR’. :slight_smile: 
[attachment=0]w600-session-0.png[/attachment]