Are all 24-pin FPC connectors compatible with XIAO eInk boards?

I’m experimenting with the XIAO eInk Expansion Board V2and noticed it uses a 24-pin FPC connector for the ePaper display.

I assumed matching the pin count and pitch would be enough, but now I’m seeing there are also differences like:

  • contact orientation

  • cable thickness

  • locking mechanism style

  • connector height/profile

Some replacement cables physically fit but don’t always behave reliably.

For people who work with these ePaper/FPC setups regularly, how do you usually verify compatibility before ordering replacement cables or displays?

Do you mainly compare datasheets, or are there standard FPC specs that matter most in practice?

In most FPC ribbon setups, compatibility is not just about pin count but also contact type, locking style, and cable thickness.

I got a useful reference for understanding the specifications of different FPC Connectors .

I am still confused which one is suitable for XIAO eInk Expansion Board V2 without any doubt.

These mechanical differences are usually what cause “fits but doesn’t work properly” issues in small boards.

Hi there,

SO I have used it on a prototype, The SMD version ,

Here is the full monty , from our notes…YMMV

Physical Connector Specifications

The FPC (Flexible Printed Circuit) connector featured on the Seeed Studio XIAO ePaper Driver Board V2 is built to industry standards for small-to-medium ePaper (eInk) displays.

Key Technical Specifications

If you are looking for compatible displays, extension cables, or replacement parts, you will need to match these parameters:

  • Pin Count: 24 pins
  • Pitch: $0.5\text{ mm}$ (The center-to-center distance between adjacent pins).
  • Connection Style: Surface Mount Device (SMD), Horizontal Right-Angle.
  • Actuator Type: Zero Insertion Force (ZIF) flip-lock or slider mechanism. This allows you to slide the flexible cable in easily without resistance, then clamp it down securely to make contact.
  • Contact Type: Typically Top Contact or Dual-Contact orientation (meaning the metal trace fingers on the ePaper flex cable must face upward or match the internal contact layout of the socket).

What Type of Cable Does it Accept?

The connector interfaces directly with a Flexible Flat Cable (FFC) or Flexible Printed Circuit (FPC) ribbon attached to the display.

  • Thickness Compatibility: Standard $0.3\text{ mm}$ thick FPC/FFC cable ends (often reinforced with a stiffener tape at the contact interface).
  • Common Standard: This 24-pin, $0.5\text{ mm}$ pitch configuration is the absolute most common standard used by ePaper manufacturers like E-Ink Corp, Good Display, and Adafruit, making it highly cross-compatible with various panel models.

the Good Display is what I went with. I have a picture of the prototype somewhere, i’ll post it up, it did work well with a 8 Inch cable.

HTH
GL :slight_smile: PJ :v:

Good question — for FPC connector compatibility, pin count and pitch matching is necessary but definitely not sufficient, as you’ve found. A few practical things that matter most in real-world use:

  • Contact orientation (top-contact vs bottom-contact FPC) — this trips people up constantly since it’s not always obvious from a quick look
  • Locking mechanism type (ZIF vs non-ZIF) — a ZIF connector needs a cable designed for it; forcing a non-ZIF cable in can damage contacts
  • Cable stiffener thickness — if the cable’s stiffener doesn’t match what the connector’s locking mechanism expects, it can seat but make unreliable contact under vibration

Best practice is to always cross-check the actual connector datasheet (not just the cable’s) for these mechanical specs, not just electrical pinout, since two connectors can look identical but behave differently.

On a related note, for anyone comparing connector types more broadly, this is a decent general reference on Card Edge Connectors.