Attempting to install ardupy-aip in Python 3.11.1 returns an error…
pip3 install --upgrade ardupy.aip
Collecting ardupy.aip
Using cached ardupy_aip-1.0.0-py2.py3-none-any.whl (35 kB)
Collecting pyusb (from ardupy.aip)
Using cached pyusb-1.2.1-py3-none-any.whl (58 kB)
Collecting demjson (from ardupy.aip)
Using cached demjson-2.2.4.tar.gz (131 kB)
Preparing metadata (setup.py) ... error
error: subprocess-exited-with-error
× python setup.py egg_info did not run successfully.
│ exit code: 1
╰─> [1 lines of output]
error in demjson setup command: use_2to3 is invalid.
[end of output]
note: This error originates from a subprocess, and is likely not a problem with pip.
error: metadata-generation-failed
× Encountered error while generating package metadata.
╰─> See above for output.
note: This is an issue with the package mentioned above, not pip.
hint: See above for details.
Any help would be appreciated.
Gregwa