Hello experts,
I am trying to build the bootloader for the Arduino here on Git Hub
but I receive the error belows and also do not know how to build the bootloader. Let me know what I am missing? and how to build this project successfully?
C:\NB-IoT_Projects\ArduinoCore-imxrt\build>cmake … -DPROJ=Blink -DTOOLCHAIN=“C:/Program Files (x86)/GNU Arm Embedded Toolchain/10 2020-q4-major/bin” -DBOARD=arch_mix -DCPU=MIMXRT1062DVL6B
– Building for: NMake Makefiles
– Check for cross compile toolchain …
– Using C:/Program Files (x86)/GNU Arm Embedded Toolchain/10 2020-q4-major/bin toolchain
– The C compiler identification is GNU 10.2.1
– The CXX compiler identification is GNU 10.2.1
– The ASM compiler identification is GNU
– Found assembler: C:/Program Files (x86)/GNU Arm Embedded Toolchain/10 2020-q4-major/bin/arm-none-eabi-gcc.exe
– Detecting C compiler ABI info
CMake Error: Generator: execution of make failed. Make command was: nmake /nologo cmTC_3269f\fast &&
– Detecting C compiler ABI info - failed
– Detecting C compile features
– Detecting C compile features - done
– Detecting CXX compiler ABI info
CMake Error: Generator: execution of make failed. Make command was: nmake /nologo cmTC_3f14c\fast &&
– Detecting CXX compiler ABI info - failed
– Detecting CXX compile features
– Detecting CXX compile features - done
MIMXRT1062DVL6B
MIMXRT1062
Project: Blink
TOOLCHAIN=C:/Program Files (x86)/GNU Arm Embedded Toolchain/10 2020-q4-major/bin
CMAKE_BUILD_TYPE=Debug
CMAKE_C_COMPILER=C:/Program Files (x86)/GNU Arm Embedded Toolchain/10 2020-q4-major/bin/arm-none-eabi-gcc.exe
CMAKE_CXX_COMPILER=C:/Program Files (x86)/GNU Arm Embedded Toolchain/10 2020-q4-major/bin/arm-none-eabi-g++.exe
CMAKE_LINKER=C:/Program Files (x86)/GNU Arm Embedded Toolchain/10 2020-q4-major/bin/arm-none-eabi-ld.exe
CMAKE_OBJCOPY=C:/Program Files (x86)/GNU Arm Embedded Toolchain/10 2020-q4-major/bin/arm-none-eabi-objcopy.exe
CMAKE_OBJDUMP=C:/Program Files (x86)/GNU Arm Embedded Toolchain/10 2020-q4-major/bin/arm-none-eabi-objdump.exe
CMAKE_MAKE_PROGRAM=nmake
CMAKE_C_FLAGS= -g -Os -Wall -w -ffunction-sections -fdata-sections -fno-common -ffreestanding -fno-builtin -nostdlib --param max-inline-insns-single=500 -MMD -MP -DNDEBUG -DCPU_MIMXRT1062DVL6B -DXIP_EXTERNAL_FLASH=1 -DXIP_BOOT_HEADER_ENABLE=1 -DUSB_STACK_BM -DARDUINO_MAIN=1 -mthumb -mapcs -mcpu=cortex-m7 -mfloat-abi=hard -mfpu=fpv5-d16 -std=gnu99
CMAKE_CXX_FLAGS= -g -Os -Wall -w -ffunction-sections -fdata-sections -fno-common -ffreestanding -fno-builtin -nostdlib --param max-inline-insns-single=500 -MMD -MP -DNDEBUG -DCPU_MIMXRT1062DVL6B -DXIP_EXTERNAL_FLASH=1 -DXIP_BOOT_HEADER_ENABLE=1 -DUSB_STACK_BM -DARDUINO_MAIN=1 -mthumb -mapcs -mcpu=cortex-m7 -mfloat-abi=hard -mfpu=fpv5-d16 -std=gnu++11 -fno-rtti -fno-exceptions -fno-threadsafe-statics
LDFLAGS= -DXIP_EXTERNAL_FLASH=1 -DXIP_BOOT_HEADER_ENABLE=1 -DNDEBUG -DCPU_MIMXRT1062DVL6B -Os -Wall -fno-common -ffunction-sections -fdata-sections -ffreestanding -fno-builtin -mthumb -mapcs -std=gnu99 -mcpu=cortex-m7 -mfloat-abi=hard -mfpu=fpv5-d16 -MMD -MP --specs=nano.specs --specs=nosys.specs -Wall -fno-common -ffunction-sections -fdata-sections -ffreestanding -fno-builtin -mthumb -mapcs -Xlinker --gc-sections -Xlinker -static -Xlinker -z -Xlinker muldefs -Xlinker -Map=output.map -mcpu=cortex-m7 -mfloat-abi=hard -mfpu=fpv5-d16 -T C:/NB-IoT_Projects/PCBandGitHub/GitHubRepository/ArduinoCore-imxrt/variants/arch_mix/flexspi_nor_arduino.ld -static
CMAKE_BINARY_DIR=C:/NB-IoT_Projects/PCBandGitHub/GitHubRepository/ArduinoCore-imxrt/build
Makefile created.
– Configuring incomplete, errors occurred!
See also “C:/NB-IoT_Projects/PCBandGitHub/GitHubRepository/ArduinoCore-imxrt/build/CMakeFiles/CMakeOutput.log”.
See also “C:/NB-IoT_Projects/PCBandGitHub/GitHubRepository/ArduinoCore-imxrt/build/CMakeFiles/CMakeError.log”.
C:\NB-IoT_Projects\ArduinoCore-imxrt\build>