Arch Pro File System

I want to know if the Arch Pro has a storage unit, accessible through the Local File System, as the mbed LPC1768 has. Actually, any files I put on the USB drive, the card “sucks” it and try to run it as if it were a firmware.

Regards.

Hi,

Arch Pro doesn’t have a storage unit, so LocalFileSystem is not available. Maybe, you can use a SD card shield as a optional solution.
The mbed interface of Arch Pro and mbed LPC1768 are different. A bin file dropped into “MBED” drive will be directly put into LPC1768.

Best,