ARCH PRO File System crash

hello
on several Windows machines i’ve got the same problem :
I see the MBED Filesystem, but i cannot copy. delete add or do anything.
With a original MBED i’ve got no problems doing that.

any advice ?

thx in advance
CL

Hi CL,

The “MBED” drive of Arch Pro is different with mbed LPC1768. mbed LPC1768 contains a external flash, so extra data can be stored in the flash.
The “MBED” drive of Arch Pro is only used to download a new binary of LPC1768, new binary drop into “MBED” will disappear and run.

If you can download a new binary through “MBED” drive, please have a look at http://mbed.org/users/seeed/notebook/the-mbed-interface-of-arch-pro/.
Upgrade the firmware of mbed interface.