Apt update && apt upgrade issue on Jetpack 6.2

Hi there,

I have executed this command after few libraries’ installation “apt update && apt upgrade” and encountered the issue
“Errors were encountered while processing:
nvidia-l4t-kernel
nvidia-l4t-kernel-headers
nvidia-l4t-jetson-io
nvidia-l4t-kernel-oot-modules
nvidia-l4t-display-kernel
nvidia-l4t-kernel-oot-headers
nvidia-l4t-kernel-dtbs
E: Sub-process /usr/bin/dpkg returned an error code (1)”

How to solve this issue, can it be solved without flashing?
Attached images of system details

The error I am getting is

Looking for your earliest support, Thanks.

So that, whenever I am trying to install any package by using sudo apt install I am encountering this issue.

Hi there,

and Welcome here…

So you do Not say What hardware you have? You can use the Wiki for guidance on each particular product. FYI, the Nvidia .DTS, is NOT the Same as the Seeed XX.DTS so be sure you are using the correct files and the correct tools and the biggest is the right METHOD to do the updates, and Upgrades. I.e Can’t use the Nvidia_SDK to update you must use a Ubuntu 20.24 Hosts only.

HTH
GL :slight_smile: PJ :v:

I have NVIDIA® Jetson Orin™ NX 16GB AI Device - reComputer J4012.
And when I am trying to install some library(labelme), I am getting error "/opt/rh/gcc-toolset-14/root/usr/include/c++/14/bits/stl_vector.h:1130: std::vector<_Tp, _Alloc>::reference std::vector<_Tp, _Alloc>::operator [with _Tp = unsigned int; _Alloc = std::allocator; reference = unsigned int&; size_type = long unsigned int]: Assertion ‘__n < this->size()’ failed.
Aborted (core dumped)
"
Can you help me out in finding the root cause of this bug and guide me for solution since this issue is related to this system not library.

Hi, any update on this.
It would be huge help if anyone can help in finding root cause of this issue.

I have exactly the same error with a reServer J3011, following the instructions for flashing from the getting strated section from the seeed studio wiki.

Hi @luke111, you can refer from below url incase you are still getting subprocess error (I was getting this error after running apt update command).

dpkg fails on Ubuntu Server 22.04 LTS - Stack Overflow

And the second issue I asked was related to GCC, later on I found out it was due to internal library depedencies. I would recommand, if you are facing similar issue just cross check once your library versions.