I picked up a couple of. Rasperry Pi cameras for my Nano not realizing that Jetpack didn’t support the IMX7 chipset. I see that Ridge Run has a overlay patch to add support, but its not working so far for me. The .dtb file included is for the 2GB Nano and not the 4GB. I tried manually comparing the decompiled .dts files but there are differing phandles between them that makes copying the info from the Ridge .dts file impossible (or at least with my understanding).
So, thought i’d reach out here and see if anyone else has been successful in getting the newer RPi cameras working on the Jetson Nano module.