After amending the /boot/extlinux/extlinux.conf I can't boot

Hi @tjax .
If you want to move the system to an SD card, please do so as follows:

  1. If you want to move the system to SD card, you need to flash the JetPack OS to reComputer J1010. That is, follow the Wiki below:
  1. After successfully flashing the jetpack to the J1010, open the desktop of the J1010 and enable the SD card by following the steps in the link below.
  1. After successfully completing the second step, you can already enable the onboard SD card function. Next you need to move the system to the SD card, i.e. perform the steps in the link below.

After completing the above four steps, you can move the system to the SD card.

Please note that you cannot use the Jetson Nano image flashed on the Jetson Nano Developer Kit on the J1010. If you want to boot from an SD card on the J1010, you can only follow the steps provided above.