A few questions about the MR60BHA1

Hi everyone, I have a couple of questions about the “Sleeping Radar Demo – Realtime Display” on the MR60BHA1 wiki:

  1. In “Section 4: Graphic Display”, for the “Breathing curve”, what does the “vertical coordinate” labeled as “corresponding data” represent? Is it data related to “Amplitude”?
  2. In “Section 2: Function Setting”, does the “Save Raw Data” option save the same data shown in “Section 3: Serial Monitor”?
  3. Does the MR60BHA1 provide lower-level raw data?

Thanks in advance!

Hi there,

SO , I think they updated the Wiki so lok there too, but I believe it to be the Amplitude and distance will affect it. Yes on #2 it’s the same data.
#3 NO, I think it’s still proprietary the tech they use but plans to make it open source are in the works.
Also I hear their is a more accurate and open unit in the works. Seems a lot of Co. are offering these more and more.

I think between the Specific LAYouts of them probably some patent and copy issue rising up. :crossed_fingers:
Stay tuned.

HTH
GL :slight_smile: PJ :v:

Hi PJ_Glasso,
Thank you for your response — it helped me a lot!