Hi,
The overview diagram for the 6-mic array shows a jumper which appears to allow the use of the GPIO clock instead of the on-board 24MHz oscillator.
I have an application which requires the DAC clocks on the microphone array to be phase locked with the RPi clock, so I would like to be able to use this feature. Does anyone have any pointers for what to do to use this feature?
Hi there,
here is the schematic related with mclk_en. thanks.
Thanks for that Bill.
I think that the 2520 type oscillator sets its output to high impedance when enable is low, so I should be able to put in the missing link, drive MCLK_EN low, and then drive GCLK from the Pi. My only question is whether a 24MHz clock is feasible to send over the GPIO connector. I know that the AC108 has many possible input clocks. Could you advise on how to program its PLL for a lower frequency clock input?
Colin