5 inch 720x1280 HDMI IPS LCD Display Dimensions

Hi,

I’m very interested in the 5 inch 720x1280 HDMI IPS LCD Display (SKU:
104990442) for a project I will be doing. One thing I need to know that I
couldn’t find on the product description is how deep the screen, including
driver the board, is. The datasheet looks like it only specifies the depth
of the screen itself, not including the I/O board with the connectors. I’m
working in a tight space, so I need to know if the screen will fit. I can
see that the product description says it’s 134mm wide x 84mm tall. I just
need to know the depth dimension before I can make a decision.

Thanks,
Razik

Great, thanks! Can I also ask the same question about the 7" version
(SKU: 104990443)? I might be able to squeeze the bigger height and width if
it’s a similar depth.
-Razik

Hi

Razik


It is the same height as 5 inch.

Thanks

best rgds
Bill