We are developing a custom board based on the ODYSSEY-STM32MP157C.
It would be nice to have a 3D model of the SOM ODYSSEY-STM32MP157C. Is it available?
Thanks, Gerrit.
We open source all of the design files.
Thank you for the link! This is only a SketchUp File of the whole Odyssey STM32MP157C Evaluation board, including the SOM. What I need is a STEP file of the SOM. Would it be possible to make it also available?
To be more precise, I have the following problems using the SketchUp model:
- the included 3D model of the SOM is too undetailed, e.g. the connectors on the bottom side are missing. This would be useful to check the positions of the connectors on the carrier board. Your model is a PCB only with 3 holes and 4 cuboids for the main chips…
- for converting SketchUp to STEP you need an offcial license. When using the free STL, the textures are getting lost.
Do I have a chance to get a more detailed 3D model of the Odyssey STM32MP157C SoM? The available SketchUp-File is not really useful for me…