I have connected the Dragino shield on top of the Seeeduino (as it should(?))
I follow this tutorial: https://wiki.dragino.com/index.php?titl ... o_Mega2560
I tried the part where you could connect the TX/RX of the lotus to the shield's RX/TX but it does not work
I connected a USB UART to the debug pins of the shield
Tried putting a 2A charger to the seeeduino and seeing what it does in the serial monitor via the RX/TX but nothing changes so it is probably not a power issue
I am getting this in the arduino serial monitor when I reset the shield, so it does do something
Code: Select all
úBÿSLÆüÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿÿ
REBOOT_CAUSE_SECURITY_RESET_UNKNOWN
Neul
OK

The "AT" etc. commands return nothing, does anyone know where I am going wrong?