TFT Touch Shield Backlight

Ardiuno Compatible shields

Moderators: lily.li, salmanfarisvp, violet

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Fri Jul 05, 2019 3:58 pm

Hi,

How is it possible to modify the intensity of the backlight when you hack the touchscreen ?
Other question, is it possible to sold the D7 connection with the 5V and the one which is between them ?

Regards,

Alexis

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Fri Jul 05, 2019 4:36 pm

Hi there~

1. No, you can not. I tested it with PWM. It does not work. It only supports on and off.

2. The mid one is the one connected with LCD. The default is VCC. I does not make sure to cut the VCC connection and then  connect to D7 which is connected with VCC. 



Thanks

best rgds
Bill


Post Reply