NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

If you have a new product idea, let us know here!

Moderators: lily.li, violet, jeremy882, ming.wen, lakshanthad, elaine.wu

yokonav
Pre-kindergarten
Pre-kindergarten
Posts: 19
Joined: Mon Feb 09, 2015 9:10 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by yokonav » Wed Mar 20, 2019 12:04 am

jeremy882 wrote:
Tue Mar 19, 2019 5:14 pm
yokonav wrote:
Fri Mar 15, 2019 7:16 am
This looks amazing with a lot of possibilities! If we are using it with Raspberry Pi, we do not need wifi, bluetooth, sd card module but of course as a standalone unit we might need it. I was working on the "Recognition of Activities of Daily Lives (ADL)" and there was requirement for a 3-axis accelerometer. The problem is: if we use 3-axis accelerometer grove module, for better result it should be mounted parallel to the board. It would be very helpful to add a 3-axis accelerometer on the board itself which I think would not take much space. It will be beneficial for other use cases like auto-rotate lcd screen, free fall detection (to save data before it crashes!), almost all robotics projects (auto driving) needs it. I am eager to try it out soon!
Thanks for the suggestion, a 3-axis accelerometer sensor integrated on the board is surely more convenient than using Grove. Will try to find a cost-effective one so that not adding too much cost for our users, do you have any recommendation for the 3-Axis accelerometer sensor?
I think ST LIS2DH12 is low-cost and ultra-low-power and also useful for gesture recognition, free fall and wake up detection and many other features.

jeremy882
Staff
Staff
Posts: 47
Joined: Sun Apr 08, 2018 12:40 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by jeremy882 » Wed Mar 20, 2019 5:24 pm

marioalemn wrote:
Fri Mar 15, 2019 12:31 am
A connector for a battery pack would be great! So the battery pack could power both the HAT and the Pi itself.
For Raspbeery Pi + the AI HAT, the lithum battery would run out very rapidly :mrgreen:

elaine.wu
Pre-kindergarten
Pre-kindergarten
Posts: 17
Joined: Mon Nov 05, 2018 5:59 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by elaine.wu » Wed Mar 27, 2019 11:07 am

UPDATE: We just got the first look of this Grove AI HAT for Edge Computing and Raspberry Pi based on the Sipeed MAIX-I, including LCD and Camera Interfaces, connectors for Digital, I2C, UART and Analog.
Don’t hesitate to share your thoughts and ideas with us in this forum! Let us know what features you would like to see and have the chance of making it to the final product.
ImageImage

yokonav
Pre-kindergarten
Pre-kindergarten
Posts: 19
Joined: Mon Feb 09, 2015 9:10 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by yokonav » Wed Mar 27, 2019 4:54 pm

Wow, looking cool! Hoping to see an accelerometer in the next revision and want to try it out soon.

julie.weber
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Tue Apr 02, 2019 3:49 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by julie.weber » Tue Apr 02, 2019 4:05 pm

jeremy882 wrote:
Wed Mar 20, 2019 5:24 pm
marioalemn wrote:
Fri Mar 15, 2019 12:31 am
A connector for a battery pack would be great! So the battery pack could power both the HAT and the Pi itself.
For Raspbeery Pi + the AI HAT, the lithum battery would run out very rapidly :mrgreen:
I think it's a good idea to add a connector for a battery pack, not to power the board with the battery only but to have an UPS for short power failure. It could be very useful to prevent data corruption.

baqwas
Pre-kindergarten
Pre-kindergarten
Posts: 37
Joined: Tue Dec 29, 2015 4:28 am

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by baqwas » Thu Apr 04, 2019 9:08 pm

Hello,

Is there a release schedule for the revisions posted (for easy lookup) and order placement?

Thanks.

jeremy882
Staff
Staff
Posts: 47
Joined: Sun Apr 08, 2018 12:40 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by jeremy882 » Mon Apr 08, 2019 2:59 pm

Hi Guys,

Thanks for all the wonderful ideas! Here is an update about things we are going to add to the next version.

1. There AI HAT can power Raspberry Pi directly. Just use the onboard switch to switch power mode.
2. There will be a microphone on board, the same microphone as the Sipeed 6+1 micarray.
3. There will be an ADXL345, 3-Axis Accelerometer on board. We choose this one because there is already a Grove version of the sensor, the software is ready, easier to get a sample, and also lower cost.
4. There will be a user button, and the boot LED can be used as user LED.
6. The 40-Pin interface will be changed to SMT female header.
5. The JTAG package will be smaller.

We will finish the layout in a week, and get samples of the second version in the week of 22-Apr. If everything goes well, we will do pre-order in early May.

Welcome to more ideas about how to using Grove with this HAT~

jeremy882
Staff
Staff
Posts: 47
Joined: Sun Apr 08, 2018 12:40 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by jeremy882 » Mon Apr 08, 2019 3:01 pm

baqwas wrote:
Thu Apr 04, 2019 9:08 pm
Hello,

Is there a release schedule for the revisions posted (for easy lookup) and order placement?

Thanks.
Hi baqwas,

We will finish the layout in a week, and get samples of the second version in the week of 22-Apr. If everything goes well, we will do pre-order in early May. Thank you~

seeed622
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Thu Jul 26, 2018 9:56 pm

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by seeed622 » Fri Apr 19, 2019 1:15 am

This processor has an amazing APU ( audio processing unit ) that is capable of handling ( 8 ) 192 khz audio streams with hardware accelerated FWT processing. It would be a shame not to have a way to access those features via I2S. It would make an amazing engine for processing high-end audio, especially in combination with the Pi.

User avatar
hitmanarky
Pre-kindergarten
Pre-kindergarten
Posts: 17
Joined: Sat Apr 06, 2019 12:22 am

Re: NEW Releasing: Grove AI HAT for Edge Computing and Look forward to your ideas!

Post by hitmanarky » Wed Apr 24, 2019 12:59 am

Please consider adding a camera that is ideal for future machine vision applications. At the moment Pregius Gen 3 Global Shutter CMOS is the my favorite. :)

https://www.sony-semicon.co.jp/products ... egius.html

What do you expect from a good machine vision camera?

* Accurate color reproduction
* No chromatic aberration
* Good low light performance
* Interchangeable lens with mount system
* High frame rate upto 120 fps
* Ability to access and change the parameters of the camera settings (white balance etc)

For conservation projects, the embedded vision camera need specific requirements.

Camera with IR cut filter / IR-white-red flash /star light camera are ideal.

Post Reply