Core v2 Alexa project

Hi,


  1. Can the name be changed from snowboy to something else

    yes, please refer to Q2 of the FAQ, http://wiki.seeedstudio.com/ReSpeaker_Core_v2.0/#faqs


  2. Can the voice be changed, and if so how/what voice font type do I need SAPI?

    do you mean the accent?


  3. the Box drawings in this link seems to have In the zip folder three STL files. However, the Bottom, and the Trumpet fixed ring both look the same. I don’t see that actual bottom plate.

    I checked the files and looks like bottom and trumpet fixed ring are the same shape. I will feedback to engineer. By the way, it shall work for the case assemby even they are the same.


  4. Is there a cover for this to go over the circuit board

    No, please make sure leave space for the led, mics and button if you want to design a cover.


  5. oh, and does the Core v2 work with UHS-3 SD cards?

    It shall support, the the speed can’t be achieved as UHS-3 standard. we do not test it yet. thanks.



    Bill