I couldn’t get the answer from the wiki. It looks like a battery is required for the RePhone to work. When I connect it to USB power without a battery the LED is red.
It looks like a battery is mandatory. Is this correct?
Yes, without battery you can’t work.
Hi,
So, can we purchase the battery in seeed shop?
What SKU is the battery for this module?
Thanks,
Roberto
Hi,
I found that the module can (in fact it is right now in front of my eyes) work without battery.
All you have to do is power the module with a good 3.3V power source. I have an old ATX power supply giving more than 3A and it’s working OK. Use pin 6 for GND and pin 3 for +3V and also connect me module to your PC (this is very important).
Now you can enjoy your module without a battery, even with a SIM connected seems to be working OK (i.e. I’ve been able to send SMSs).
Regards,
Roberto.