noise suppression with librespeaker in RespeakerCorev2

info about ReSpeaker series products

Moderators: lily.li, violet, salmanfarisvp, seth.welday

chdyejiewei
Pre-kindergarten
Pre-kindergarten
Posts: 22
Joined: Mon Oct 15, 2018 3:11 pm

Re: noise suppression with librespeaker in RespeakerCorev2

Post by chdyejiewei » Wed Dec 05, 2018 4:34 pm

How do you think that if we capture audio via alsa api and redirect the processed audio stream with alsa-aloop? Then snips or other ASRs can capture the processed audio stream easily.

cinettoa
Pre-kindergarten
Pre-kindergarten
Posts: 30
Joined: Fri Jul 20, 2018 10:33 am

Re: noise suppression with librespeaker in RespeakerCorev2

Post by cinettoa » Thu Dec 06, 2018 10:34 am

Hi Jerry,

This way could be god. the more general the best so to adapt to future available ASR API.

Are you going to develop a new respeaker release for this?

chdyejiewei
Pre-kindergarten
Pre-kindergarten
Posts: 22
Joined: Mon Oct 15, 2018 3:11 pm

Re: noise suppression with librespeaker in RespeakerCorev2

Post by chdyejiewei » Thu Dec 06, 2018 12:15 pm

Yes, this is what we are doing.

cinettoa
Pre-kindergarten
Pre-kindergarten
Posts: 30
Joined: Fri Jul 20, 2018 10:33 am

Re: noise suppression with librespeaker in RespeakerCorev2

Post by cinettoa » Thu Dec 06, 2018 2:20 pm

sounds good! do you a timeline for the new release?

chdyejiewei
Pre-kindergarten
Pre-kindergarten
Posts: 22
Joined: Mon Oct 15, 2018 3:11 pm

Re: noise suppression with librespeaker in RespeakerCorev2

Post by chdyejiewei » Wed Dec 12, 2018 4:23 pm

Hi,

The new release is still need some time to go, but I can send you a test version, you can download from this link:
https://v2.fangcloud.com/share/11a20219 ... f8?lang=en

Install the lib:
tar -jxvf librespeaker.tar.bz2
sudo dpkg -i librespeaker_2.1.2-build181212_armhf.deb
sudo dpkg -i librespeaker-dev_2.1.2-build181212_armhf.deb

Compile the example:
g++ alsa_aloop_test.cc -o alsa_aloop_test -lrespeaker -lsndfile -fPIC -std=c++11 -fpermissive -I/usr/include/respeaker/ -DWEBRTC_LINUX -DWEBRTC_POSIX -DWEBRTC_NS_FLOAT -DWEBRTC_APM_DEBUG_DUMP=0 -DWEBRTC_INTELLIGIBILITY_ENHANCER=0

/** @example alsa_aloop_test.cc
* This is an example that shows how to redirect the processed audio stream into a specific Alsa device(Loopback PCM).
* To run this example, you have to run 'sudo modprobe snd-aloop' first. And make sure "pulseaudio" doesn't start, then
* you can use "arecord -Dhw:Loopback,1,0 -c 1 -r 16000 -f S16_LE loop_test.wav" to arecord the processed audio stream.
* Further more, you can setup a third party voice assistant to capture voice from "hw:Loopback,1,0", to run the assistant directly.
*/

Note that the header files are located in /usr/include/respeaker, and you can find how to use aloop_node in "aloop_output_node.h". The other APIs are the same as
the previous version.
And the config files are in /usr/share/respeaker

Feel free to ask me if you have any question.

Thanks,
Jerry

frederic.bost
Pre-kindergarten
Pre-kindergarten
Posts: 10
Joined: Fri Mar 23, 2018 10:22 am

Re: noise suppression with librespeaker in RespeakerCorev2

Post by frederic.bost » Wed Dec 19, 2018 7:31 am

Hi,

Thanks for this new aloop node.
This is very useful.

I got it to work with your example.
But if you let it run for sometimes, ultimately you get a long list of "underrun" error like the following ones and it stops recording at that point.
....
(145514ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
(145986ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
...

Any idea on how to fix this?
Thanks

chdyejiewei
Pre-kindergarten
Pre-kindergarten
Posts: 22
Joined: Mon Oct 15, 2018 3:11 pm

Re: noise suppression with librespeaker in RespeakerCorev2

Post by chdyejiewei » Wed Dec 19, 2018 9:27 am

"underrun" means the aloop node doesn't send the audio data to the loopback buffer on time.
If you got a long list of this, it was probably because the previous nodes didn't send the audio data to aloop node. I think something stuck "vep node" at that time. You can monitor the CPU usage with "htop" and you will find 2 threads of this example rise to 100% before "underrun" happens. We are trying to avoid this "stuck", and this example will still work after "underrun" happened.

Thanks,
Jerry

frederic.bost
Pre-kindergarten
Pre-kindergarten
Posts: 10
Joined: Fri Mar 23, 2018 10:22 am

Re: noise suppression with librespeaker in RespeakerCorev2

Post by frederic.bost » Wed Dec 19, 2018 10:02 am

Thanks for the reply.
Using htop helps the monitoring indeed.

I also tried to adapt the example as I don't need wakeup word detection but instead I look for a clean audio while capturing it live before sending it to a ASR API.
So I linked the nodes: alsa -> hybrid(agc) -> hybrid(ns) -> hybrid (vad) -> vep_1beam -> selector -> aloop
Based on my tests, it seems to be the best combination but maybe you can recommend a better one based on your experience.
I used the latest version 2.1.2 of the library and could not compile successfully with the Hybrid Create function so the multiple individual hybrid nodes:
"... undefined reference to `respeaker::HybridNode::Create(bool, int, int, int, bool, int, bool)"

In any case, after few minutes, the program generates the underrun messages and never stop doing it.
I can still record indeed but miss lots of blocks and the result is not very good any more.

Would you have any suggestions to improve my use cases?
Let me know if you need more details too.

Thanks you very much for your help,
Fred

chdyejiewei
Pre-kindergarten
Pre-kindergarten
Posts: 22
Joined: Mon Oct 15, 2018 3:11 pm

Re: noise suppression with librespeaker in RespeakerCorev2

Post by chdyejiewei » Wed Dec 19, 2018 1:49 pm

Hi,

Thanks for the feedback.
Let me explain these nodes in details:
(1)hybrid_node: this node provides NS, AGC, VAD algorithms from WebRTC lib, not the Alango, so we are more recommended to use the vep_node. What is more, you can enable NS, AGC, VAD in the same instance in your case, for examples:

Code: Select all

hybrid.reset(HybridNode::Create((bool)enable_ns, (int)ns_level, (int)agc_type, (int)agc_level, (bool)enable_vad, (int)vad_sensitivity,true));
As the more nodes you have, the more latency you will get.
(2)vep_node: this node also provides: NS, BF, AEC algorithms from Alango, and these algorithms are better than the hybrid_node algorithms
(3)snowboy_1b_node: this node not only provides KWS, but also provides AGC and VAD. You can call respeaker->GetVad() to get VAD status(Please see pulse_snowboy_1b_multi_hotword_vad_test.cc for more detail).

Back to your case, I still recommend to use the example I provided: alsa->vep->snowboy->aloop, you can just ignore the KWS part.
And can you send me a debug log from your program when the endless "underrun" happen?

Thanks,
Jerry.

frederic.bost
Pre-kindergarten
Pre-kindergarten
Posts: 10
Joined: Fri Mar 23, 2018 10:22 am

Re: noise suppression with librespeaker in RespeakerCorev2

Post by frederic.bost » Thu Dec 20, 2018 2:28 am

Thanks
That was very useful information which helped me a lot.

So I went back to your example but still have the "underrun" issue.
I just realized that it starts when i use aplay (or play) to play the recording from another SSH session.

Here is the use case:
- On a first SSH session, I run your example as following:
$ sudo ./alsa_aloop_test -t CIRCULAR_6MIC_7BEAM -g 5
using snowboy kws
AGC = -5
(48ms)INFO -- Sample rate is 48000 [alsa_collector_node.cc:337]
(48ms)DEBUG -- Buffer time max is 341334 [alsa_collector_node.cc:355]
(196ms)DEBUG -- Chunk size is 1920 [alsa_collector_node.cc:396]
(196ms)INFO -- Finish setting Alsa hardware params. [alsa_collector_node.cc:399]
(206ms)DEBUG -- VepAecBeamformingNode read microphone config file successfully. [vep_aec_beamforming_node.cc:181]
(207ms)DEBUG -- VEP: I need 604248 bytes of memory in memory region 1 to work.
[vep_aec_beamforming_node.cc:207]
(207ms)DEBUG -- VEP: I need 0 bytes of memory in memory region 2 to work.
[vep_aec_beamforming_node.cc:207]
(211ms)DEBUG -- VepAecBeamformingNode input: channels 8 rate 16000, output: channels 3 rate 16000 [vep_aec_beamforming_node.cc:340]
(212ms)INFO -- VepAecBeamformingNode thread started. [vep_aec_beamforming_node.cc:342]
(238ms)INFO -- Snowboy1bDoaKwsNode enabled AGC. [snowboy_1b_doa_kws_node.cc:276]
(238ms)DEBUG -- Snowboy1bDoaKwsNode input: channels 3 rate 16000, output: channels 1 rate 16000 [snowboy_1b_doa_kws_node.cc:291]
(238ms)INFO -- Snowboy1bDoaKwsNode thread started. [snowboy_1b_doa_kws_node.cc:293]
(241ms)INFO -- Finish setting Aloop [aloop_output_node.cc:225]
(242ms)INFO -- MaxBlockDelayTime is actually set to: 6 * 40ms = 240ms. [aloop_output_node.cc:343]
num channels: 1, rate: 16000
collector: 1, vep_1beam: 0, snowboy_kws: 0, aloop: 0
collector: 2, vep_1beam: 0, snowboy_kws: 0, aloop: 0
.......

- On a second SSH session, I record as following:
$ sox -t alsa hw:Loopback,1,0 -t wavpcm -c 1 -b 16 -r 16000 -e signed-integer --endian little - silence 1 0.1 1% 1 1.0 3% > aloop_test.wav

Everything works fine so I play it to listen to it:
$ aplay aloop_test.wav

- Then on the screen of the first session, it starts displaying the following underrun message non-stop and I can not record any more:
(17988ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
(18473ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
collector: 3, vep_1beam: 0, snowboy_kws: 0, aloop: 0
(18960ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
collector: 0, vep_1beam: 0, snowboy_kws: 0, aloop: 0
(19432ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
collector: 1, vep_1beam: 0, snowboy_kws: 0, aloop: 0
(19907ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
collector: 0, vep_1beam: 0, snowboy_kws: 0, aloop: 0
(20391ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
(20867ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
collector: 1, vep_1beam: 1, snowboy_kws: 0, aloop: 0
(21341ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
collector: 0, vep_1beam: 0, snowboy_kws: 0, aloop: 0
(21821ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
collector: 1, vep_1beam: 0, snowboy_kws: 0, aloop: 0
(22296ms)DEBUG -- Try to recovery from underrun [aloop_output_node.cc:277]
collector: 0, vep_1beam: 0, snowboy_kws: 0, aloop: 0

Am I doing anything wrong?

Thanks,
Fred

Post Reply