Does mic_array.get_direction (from mic_array.py) work?

info about ReSpeaker series products

Moderators: lily.li, violet, seth.welday

Post Reply
ed.sutter
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Fri Mar 08, 2019 4:10 am

Does mic_array.get_direction (from mic_array.py) work?

Post by ed.sutter » Fri Mar 08, 2019 4:44 am

Hi,
UPDATE: I changed the subject/text to be more specific to my problem...

I purchased a ReSpeaker Circular Array (Pi-Hat) with 6 microphones.
I've walked through the installation (hardware and packages) as outlined on
your site (...ReSpeaker_6-Mic_Circular_Array_kit_for_Raspberry_Pi...)
Excellent "how-to" page by the way...

I've tried two different sections of that page so far...

1. ALSA API
I skipped down to the ALSA API section and had immediate success with
alsa_snips_1b_test.cc. It clearly detects "hey snips" and reports the DOA.
Cool!

2. DOA without keywords (using vad_doa.py)
The VAD portion of this seems to work but the value returned by mic.get_direction()
has no consistency, and it seems to cause the program to hang quite often.
Note that I did change CHANNELS to 8.

Since the ALSA API stuff works great, that kinda tells me that I have things installed properly.
Any idea why the (simpler) DOA without keywords stuff doesn't seem to work?

jtt083
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Mon Mar 11, 2019 9:31 am

Re: Does mic_array.get_direction (from mic_array.py) work?

Post by jtt083 » Tue Mar 12, 2019 9:09 am

I have the same issue with the project DOA without keywords (using vad_doa.py).
The value returned by mic.get_direction()
has no consistency, and it seems to cause the program to hang quite often.

ed.sutter
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Fri Mar 08, 2019 4:10 am

Re: Does mic_array.get_direction (from mic_array.py) work?

Post by ed.sutter » Fri Mar 15, 2019 4:29 am

Apparently the 4-mic array has similar problems based on this post...

viewtopic.php?f=87&t=9314
Looks like that guy just gave up.

I've followed all the installation steps, so can someone from SEEED suggest something?

bill.yu
Elementary-4
Elementary-4
Posts: 489
Joined: Mon Apr 02, 2018 11:05 am

Re: Does mic_array.get_direction (from mic_array.py) work?

Post by bill.yu » Fri Mar 15, 2019 6:18 pm

Hi there,

The doa without keywords work well with respeaker 4 mic pi hat, i tested it just now. you can see the result from viewtopic.php?f=87&t=9314

The doa without keywords with respeaker 6 mic pi hat, please do below changes. but it is still not very stable.

1. vad_doa.py:change the channels to 8

RATE = 16000
CHANNELS = 8
VAD_FRAMES = 10 # ms
DOA_FRAMES = 200 # ms

2. mic_arrray.py: change the mic distance to 0.094 and MIC_GROUP = [[0, 3], [1, 4], [2, 5]]

MIC_DISTANCE_6P1 = 0.094
MAX_TDOA_6P1 = MIC_DISTANCE_6P1 / float(SOUND_SPEED)

def get_direction(self, buf):
best_guess = None
if self.channels == 8:
MIC_GROUP_N = 3
MIC_GROUP = [[0, 3], [1, 4], [2, 5]]

ed.sutter
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Fri Mar 08, 2019 4:10 am

Re: Does mic_array.get_direction (from mic_array.py) work?

Post by ed.sutter » Fri Mar 15, 2019 9:33 pm

@bill.yu... Yes, thanks, that made a significant difference in the DOA results!
Unfortunately it does still randomly hang. Do you see it hang?

jtt083
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Mon Mar 11, 2019 9:31 am

Re: Does mic_array.get_direction (from mic_array.py) work?

Post by jtt083 » Tue Mar 19, 2019 4:20 pm

I follow the step to modify the code ,and it is often randomly hang . And the output result isn't stable like the 4-mic Array you post in another article.

bill.yu
Elementary-4
Elementary-4
Posts: 489
Joined: Mon Apr 02, 2018 11:05 am

Re: Does mic_array.get_direction (from mic_array.py) work?

Post by bill.yu » Wed Mar 20, 2019 10:24 am

Hi there,

We are working on the issue and keep you posted.

User avatar
bestlux
Kindergarten
Kindergarten
Posts: 85
Joined: Wed Jan 30, 2019 11:51 am

Re: Does mic_array.get_direction (from mic_array.py) work?

Post by bestlux » Tue Mar 26, 2019 4:13 pm

hello,
pls switch your mic_array.py with the following code. Then it can work with 6-mic array.
The mic array detects all the voice source in the environment and it is also reflected in the results of the program.so the results seem to be mixed with random numbers sometimes…but you can still find the main source of voice in the results. As a follow-up, you need to do numerical processing if you just want to catch the one target.

Code: Select all

import pyaudio
import Queue
import threading
import numpy as np
from gcc_phat import gcc_phat
import math


SOUND_SPEED = 343.2

MIC_DISTANCE_6P1 = 0.09218
MAX_TDOA_6P1 = MIC_DISTANCE_6P1 / float(SOUND_SPEED)

MIC_DISTANCE_4 = 0.08127
MAX_TDOA_4 = MIC_DISTANCE_4 / float(SOUND_SPEED)



class MicArray(object):

    def __init__(self, rate=16000, channels=8, chunk_size=None):
        self.pyaudio_instance = pyaudio.PyAudio()
        self.queue = Queue.Queue()
        self.quit_event = threading.Event()
        self.channels = channels
        self.sample_rate = rate
        self.chunk_size = chunk_size if chunk_size else rate / 100

        device_index = None
        for i in range(self.pyaudio_instance.get_device_count()):
            dev = self.pyaudio_instance.get_device_info_by_index(i)
            name = dev['name'].encode('utf-8')
            print(i, name, dev['maxInputChannels'], dev['maxOutputChannels'])
            if dev['maxInputChannels'] == self.channels:
                print('Use {}'.format(name))
                device_index = i
                break

        if device_index is None:
            raise Exception('can not find input device with {} channel(s)'.format(self.channels))

        self.stream = self.pyaudio_instance.open(
            input=True,
            start=False,
            format=pyaudio.paInt16,
            channels=self.channels,
            rate=int(self.sample_rate),
            frames_per_buffer=int(self.chunk_size),
            stream_callback=self._callback,
            input_device_index=device_index,
        )

    def _callback(self, in_data, frame_count, time_info, status):
        self.queue.put(in_data)
        return None, pyaudio.paContinue

    def start(self):
        self.queue.queue.clear()
        self.stream.start_stream()


    def read_chunks(self):
        self.quit_event.clear()
        while not self.quit_event.is_set():
            frames = self.queue.get()
            if not frames:
                break

            frames = np.fromstring(frames, dtype='int16')
            yield frames

    def stop(self):
        self.quit_event.set()
        self.stream.stop_stream()
        self.queue.put('')

    def __enter__(self):
        self.start()
        return self

    def __exit__(self, type, value, traceback):
        if value:
            return False
        self.stop()

    def get_direction(self, buf):
        best_guess = None
        if self.channels == 8:
            MIC_GROUP_N = 3
            MIC_GROUP = [[0, 3], [1, 4], [2, 5]]

            tau = [0] * MIC_GROUP_N
            theta = [0] * MIC_GROUP_N

            buf = np.fromstring(buf, dtype='int16')
            for i, v in enumerate(MIC_GROUP):
                tau[i], _ = gcc_phat(buf[v[0]::8], buf[v[1]::8], fs=self.sample_rate, max_tau=MAX_TDOA_6P1, interp=1)
                theta[i] = math.asin(tau[i] / MAX_TDOA_6P1) * 180 / math.pi

            min_index = np.argmin(np.abs(tau))
            if (min_index != 0 and theta[min_index - 1] >= 0) or (min_index == 0 and theta[MIC_GROUP_N - 1] < 0):
                best_guess = (theta[min_index] + 360) % 360
            else:
                best_guess = (180 - theta[min_index])

            best_guess = (best_guess + 30 + min_index * 60) % 360
        elif self.channels == 4:
            MIC_GROUP_N = 2
            MIC_GROUP = [[0, 2], [1, 3]]

            tau = [0] * MIC_GROUP_N
            theta = [0] * MIC_GROUP_N
            for i, v in enumerate(MIC_GROUP):
                tau[i], _ = gcc_phat(buf[v[0]::4], buf[v[1]::4], fs=self.sample_rate, max_tau=MAX_TDOA_4, interp=1)
                theta[i] = math.asin(tau[i] / MAX_TDOA_4) * 180 / math.pi

            if np.abs(theta[0]) < np.abs(theta[1]):
                if theta[1] > 0:
                    best_guess = (theta[0] + 360) % 360
                else:
                    best_guess = (180 - theta[0])
            else:
                if theta[0] < 0:
                    best_guess = (theta[1] + 360) % 360
                else:
                    best_guess = (180 - theta[1])

                best_guess = (best_guess + 90 + 180) % 360


            best_guess = (-best_guess + 120) % 360

             
        elif self.channels == 2:
            pass

        return best_guess


def test_4mic():
    import signal
    import time

    is_quit = threading.Event()

    def signal_handler(sig, num):
        is_quit.set()
        print('Quit')

    signal.signal(signal.SIGINT, signal_handler)
 
    with MicArray(16000, 4, 16000 / 4)  as mic:
        for chunk in mic.read_chunks():
            direction = mic.get_direction(chunk)
            print(int(direction))

            if is_quit.is_set():
                break


def test_8mic():
    import signal
    import time
    from pixel_ring import pixel_ring

    is_quit = threading.Event()

    def signal_handler(sig, num):
        is_quit.set()
        print('Quit')

    signal.signal(signal.SIGINT, signal_handler)
 
    with MicArray(16000, 8, 16000 / 4)  as mic:
        for chunk in mic.read_chunks():
            direction = mic.get_direction(chunk)
            pixel_ring.set_direction(direction)
            print(int(direction))

            if is_quit.is_set():
                break

    pixel_ring.off()


if __name__ == '__main__':
    # test_4mic()
    test_8mic()

Post Reply