hello, I have a probleme when i upload my skech
Arduino: 1.8.4 (Windows 10), Card: "Wio GPS Board"
CAUTION: The category '' in the FlashStorage library is invalid. Definition on: 'Uncategorized'
The sketch uses 20104 bytes (7%) of program storage space. The maximum is 262144 bytes.
An error occurred while uploading the sketch
This report could be more detailed with
the option "Show detailed results of the compilation"
activated in File -> Preferences.
help
Moderators: lily.li, violet, seth.welday
-
- Pre-kindergarten
- Posts: 3
- Joined: Sun Jan 13, 2019 11:12 pm
Re: help
Hello, I always have the same problem. can not the computer also cause worries? I have a dual core hp with windows 10.
-
- Pre-kindergarten
- Posts: 4
- Joined: Wed Nov 27, 2019 1:17 pm
Re: help
Family and friends are often the first line of defense in the fight against depression. That’s why it’s important to understand the signs and symptoms of depression. You may notice the problem in a depressed loved one before they do, and your influence and concern can motivate them to seek help.