Wio GPS Board battery connector

Simplify IoT Development.

Moderators: lily.li, violet, seth.welday

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 56
Joined: Mon Jun 03, 2019 10:58 am

Wio GPS Board battery connector

Post by Anonymous » Thu Apr 18, 2019 8:13 pm

Hi,

today I bought two "Wio GPS Board v1.4 05/15/2017" and wonder which
connector I will need to connect a battery to the board.

All LiPo batteries I have on hand have a slightly bigger JST connector
not fitting into the JST connector on the board.

On http://wiki.seeedstudio.com/wio_gps_board/ the connector is described
as "JST 1.0 connecter for battery", in the schmematic I read
''JST-2P-SMD-90D".

Unfortunately I could not find out from your documentation and by
internet research what the exact specification / supplier part number of
this connector is and what item I need to order to connect a battery.

Please let me know which connector fits and if you know a shop where I
can buy batteries already having the right connector or an adapter.

Thank you in advance for your help!

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Fri Apr 19, 2019 10:54 am

Hi there,It is JST1.0 2 pin connector. 

JST-2P-SMD-90D stands for the JST1.0 2pin connector. We can change the name as JST1.0 2 pins and eliminate the confusion in future products. the pin distance is 1.0mm. you can refer to below link for the cables.

https://www.aliexpress.com/store/produc ... 18fdl91c4a  Thanksbest rgdsBill

Post Reply