RFBee firmware updating

Hi there,

Did some test, and see the updating of google code r27.

Changes:
1.Set rfbee into proper state after tx,rx, as in seeed v1.03.
2. Remove the delay(5) after CCx.Strobe(CCx_STX) in transmitData().

Reason:
ATCF0~3 all works now.

Issues:
The data length you send to the rfbee should be the same as the threshold every
time. Otherwise, the receiving rfbee will receive invalid data endlessly as rich has met.

The problem may exist in:
Transmit process.(As I use v1.03 as transmitter, v1.1_r26 as receiver, it works
ok). And I dont think it is the interuption by the other signal in ISM surrounding us.

Regards,

-Icing