GPRS Shield v3 questions

Ardiuno Compatible shields

Moderators: lily.li, salmanfarisvp, violet

Post Reply
soloandrea85
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Wed Mar 11, 2015 1:13 am

GPRS Shield v3 questions

Post by soloandrea85 » Thu Apr 14, 2016 6:32 am

I'm using your gprs shield in many projects.

But i have some few questions about it:

1. Wiki:
I don't understand why the wiki of the V2 is different by the V3 version of the shield... the v2 is more accurate and rich of informations.

2. Powering ON:
Around the wiki and forum you say to solder the JMP pad... but i'm using the V3 unsoldered and it will power up via arduino... so... which is the exact difference between solder and unsoldering this pad?

3. Libraries:
- Which is the difference between GPRS_Shield_Suli and GPRS_SIM900? Which is the best? Which should I use?
- Which is the "lighter" in terms of allocated byte in the arduino?

4. Firmware:
The simcom900 is a little bit slow... should i upgrade the firmware? How? Do you have a tutorial?

5. HTTP GET:
Can you add the support for the http get request?
I'm talking about this AT commands: HTTPINIT - HTTPPARA - HTTPACTION

Thanks for your support

kavi
Staff
Staff
Posts: 305
Joined: Tue Dec 09, 2014 12:06 pm

Re: GPRS Shield v3 questions

Post by kavi » Tue Apr 19, 2016 7:41 pm

1.The difference between Gprs Shiled v2.0 and the Gprs Shiled v3.0 is change in the arduino socket to the latest Arduino Uno standard. Except this, all the features are same with the Gprs Shiled v2.0.

2.Already the JMP pads are connected to the GPRS shield v3.0.So, you don't need to solder it separately.

3.Please find the description of Suli in the following link (https://github.com/Seeed-Studio/Suli#what-is-suli).

The GPRS_SIM900 library Sketch(i.e GPRS_Callup) uses 20% of program storage space and GPRS_SIM900_Suli library Sketch(i.e GPRS_Callup) uses 26% of program storage space.

4.Please find the following link to the zip file (SIM900 firmware and tool(firmware:1137B08SIM900M64_ST) for firmware upgrade) to the GPRS shield v3.0wiki resource page.

soloandrea85
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Wed Mar 11, 2015 1:13 am

Re: GPRS Shield v3 questions

Post by soloandrea85 » Wed May 16, 2018 5:53 pm

Hi

Could you tell me what is the right AT commands (from start to end) for have an HTTP GET request?

Regards

hong.jiang
Staff
Staff
Posts: 200
Joined: Tue Apr 17, 2018 11:03 am

Re: GPRS Shield v3 questions

Post by hong.jiang » Fri Aug 10, 2018 10:59 am

Hi:
AT Commands for HTTP Application mainly have the following:
AT+HTTPINT
AT+HTTPTERM
AT+HTTTPPARA
AT+HTTPDATA
AT+HTTPACTION
AT+HTTPREAD
AT+HTTPSCONT
AT+HTTPSTATUS
For detailed introduction, please refer tohttps://github.com/SeeedDocument/GPRS_S ... _v1.11.pdf

Post Reply