Set up connections between two BluetoothBee step by step
Moderators: lily.li, violet, jessie
-
- Pre-kindergarten
- Posts: 34
- Joined: Tue Jan 17, 2012 11:04 am
- Are you a staff member of seeedstudio?: yes
- Which products/projects are your favorite?: Seeeduino
Re: Set up connections between two BluetoothBee step by step
Yes,you have to use the bee shield.
The link:http://www.seeedstudio.com/depot/xbee%C ... th=132_134
The link:http://www.seeedstudio.com/depot/xbee%C ... th=132_134
Re: Set up connections between two BluetoothBee step by step
No.Tobe wrote:Yes,you have to use the bee shield.
The link:http://www.seeedstudio.com/depot/xbee%C ... th=132_134
He just need to connect VCC (3.3V), GND, RX and TX (trought a level shifter) to the Mega 2560.
Best regards from Vienna/Austria
Rony
Rony
-
- Pre-kindergarten
- Posts: 1
- Joined: Tue Jul 31, 2012 3:34 am
- Are you a staff member of seeedstudio?: no
- Which products/projects are your favorite?: Atmega
Re: Set up connections between two BluetoothBee step by step
My virus scanner picked up a threat (Mal/Generic-L) after scanning sscom32E.zip linked to on the first page of this topic.
Re: Set up connections between two BluetoothBee step by step
Hey! How can I reinitalize my BT Be to different baud rate? Using command +STD=9600 just do not work, and module stop initializing anymore.
Re: Set up connections between two BluetoothBee step by step
hello everybody,
I have problems with my BluetoothBee. I followed the steps but I could not communicate correctly with my unit. I wrote a new post but nobody replied to me. anybody can help me?
http://www.seeedstudio.com/forum/viewto ... =18&t=4161
thank you
I have problems with my BluetoothBee. I followed the steps but I could not communicate correctly with my unit. I wrote a new post but nobody replied to me. anybody can help me?
http://www.seeedstudio.com/forum/viewto ... =18&t=4161
thank you
Re: Set up connections between two BluetoothBee step by step
Hi.
Is it possible to remove the feedback messages from the Bluetooth bee?
Regards
Is it possible to remove the feedback messages from the Bluetooth bee?
Regards
-
- Pre-kindergarten
- Posts: 7
- Joined: Tue May 21, 2013 8:39 am
Re: Set up connections between two BluetoothBee step by step
I having some trouble. Not matter what mode I put the blue tooth bee in, I can't seem to find it using my android phone or my computer.
The bluetooth bee needs to be in Slave mode to connect to my computer is that correct?
Here is the response from the module.
Setting up Bluetooth link
+STWMOD=0
OK
+STNA=BluetoothBee
WORK:SLAVER
+BTSTATE:0
+BTSTATE:1
OK
+STOAUT=1
WORK:SLAVER
+BTSTATE:0
+BTSTATE:1
OK
WORK:SLAVER
+INQ=1
+BTSTATE:0
+BTSTATE:1
OK
+BTSTATE:2
Setup complete
I don't see why my phone nor my computer can see the module and i tired 3 different phones non can see it.
The bluetooth bee needs to be in Slave mode to connect to my computer is that correct?
Here is the response from the module.
Setting up Bluetooth link
+STWMOD=0
OK
+STNA=BluetoothBee
WORK:SLAVER
+BTSTATE:0
+BTSTATE:1
OK
+STOAUT=1
WORK:SLAVER
+BTSTATE:0
+BTSTATE:1
OK
WORK:SLAVER
+INQ=1
+BTSTATE:0
+BTSTATE:1
OK
+BTSTATE:2
Setup complete
I don't see why my phone nor my computer can see the module and i tired 3 different phones non can see it.
- Jacket Chen
- Staff
- Posts: 659
- Joined: Thu Jun 21, 2012 4:25 pm
- Are you a staff member of seeedstudio?: yes
- Which products/projects are your favorite?: Seeeduino Shields
- Location: China
Re: Set up connections between two BluetoothBee step by step
No,the feedback can't be deleted.mix_069 wrote:Hi.
Is it possible to remove the feedback messages from the Bluetooth bee?
Regards
Love little, love long.
-
- Pre-kindergarten
- Posts: 1
- Joined: Mon Jan 20, 2014 3:37 pm
Re: Set up connections between two BluetoothBee step by step
Hello Icing, Thanks for the information about connection between two Bluetooth bee!