How do you communicate two SEEED BLUETOOTH?

wireless communication and related Bees.

Moderators: lily.li, violet, jessie

Post Reply
newatlantisocean
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Tue Jan 08, 2013 7:25 am

How do you communicate two SEEED BLUETOOTH?

Post by newatlantisocean » Tue Jan 08, 2013 7:40 am

The Slave bluetooh shield is unable to get LED turned on by Master bluetooh shield.
How do you fix this? Here's the code:



/* Upload this sketch into Seeeduino and press reset*/
#include <SoftwareSerial.h> //Software Serial Port

#define RxD 6
#define TxD 7

#define DEBUG_ENABLED 1

String retSymb = "+RTINQ=";//start symble when there's any return
String slaveName = ";SeeedBTSlave";// caution that ';'must be included, and make sure the slave name is right.
int nameIndex = 0;
int addrIndex = 0;

String recvBuf;
String slaveAddr;

String connectCmd = "\r\n+CONN=";

SoftwareSerial blueToothSerial(RxD,TxD);

void setup()
{
Serial.begin(9600);
pinMode(RxD, INPUT);
pinMode(TxD, OUTPUT);
setupBlueToothConnection();
//wait 1s and flush the serial buffer
delay(1000);
Serial.flush();
blueToothSerial.flush();
}

void loop()
{
char recvChar;
while(1){
if(blueToothSerial.available()){//check if there's any data sent from the remote bluetooth shield
recvChar = blueToothSerial.read();
Serial.print(recvChar);
}
if(Serial.available()){//check if there's any data sent from the local serial terminal, you can add the other applications here
recvChar = Serial.read();
blueToothSerial.print(recvChar);
}
}
}

void setupBlueToothConnection()
{
blueToothSerial.begin(38400); //Set BluetoothBee BaudRate to default baud rate 38400
blueToothSerial.print("\r\n+STWMOD=1\r\n");//set the bluetooth work in master mode
blueToothSerial.print("\r\n+STNA=SeeedBTMaster\r\n");//set the bluetooth name as "SeeedBTMaster"
blueToothSerial.print("\r\n+STAUTO=0\r\n");// Auto-connection is forbidden here
blueToothSerial.print("\r\n +STPIN=0000\r\n");
delay(2000); // This delay is required.
blueToothSerial.flush();
blueToothSerial.print("\r\n+INQ=1\r\n");//make the master inquire
Serial.println("Master is inquiring!");
delay(2000); // This delay is required.

//find the target slave
char recvChar;
while(1){
if(blueToothSerial.available()){
recvChar = blueToothSerial.read();
recvBuf += recvChar;
nameIndex = recvBuf.indexOf(slaveName);//get the position of slave name
//nameIndex -= 1;//decrease the ';' in front of the slave name, to get the position of the end of the slave address
if ( nameIndex != -1 ){
//Serial.print(recvBuf);
addrIndex = (recvBuf.indexOf(retSymb,(nameIndex - retSymb.length()- 18) ) + retSymb.length());//get the start position of slave address
slaveAddr = recvBuf.substring(addrIndex, nameIndex);//get the string of slave address
break;
}
}
}
//form the full connection command
connectCmd += slaveAddr;
connectCmd += "\r\n";
int connectOK = 0;
Serial.print("Connecting to slave:");
Serial.print(slaveAddr);
Serial.println(slaveName);
//connecting the slave till they are connected
do{
blueToothSerial.print(connectCmd);//send connection command
recvBuf = "";
while(1){
if(blueToothSerial.available()){
recvChar = blueToothSerial.read();
recvBuf += recvChar;
if(recvBuf.indexOf("CONNECT:OK") != -1){
connectOK = 1;
Serial.println("Connected!");
blueToothSerial.print("Connected!");



Serial.write("1");
blueToothSerial.write("1");
blueToothSerial.print("1");
delay(2000);




break;
}else if(recvBuf.indexOf("CONNECT:FAIL") != -1){
Serial.println("Connect again!");
break;
}
}
}
}while(0 == connectOK);
}

========================================================================================================================




========================================================================================================================


/* Upload this sketch into Seeeduino and press reset*/

#include <SoftwareSerial.h> //Software Serial Port
#define RxD 6
#define TxD 7

#define DEBUG_ENABLED 1

SoftwareSerial blueToothSerial(RxD,TxD);
int led = 13;

void setup()
{
Serial.begin(9600);
pinMode(RxD, INPUT);
pinMode(TxD, OUTPUT);
setupBlueToothConnection();
pinMode(led, OUTPUT);

}

void loop()
{
char recvChar;
// while(1){
if(blueToothSerial.available()){//check if there's any data sent from the remote bluetooth shield
recvChar = blueToothSerial.read();
Serial.print(recvChar);
}
if(Serial.available()){//check if there's any data sent from the local serial terminal, you can add the other applications here
recvChar = Serial.read();
blueToothSerial.print(recvChar);
}

if (recvChar == '1') {
digitalWrite(led, HIGH); // turn the LED on (HIGH is the voltage level) }

// }

}

void setupBlueToothConnection()
{
blueToothSerial.begin(38400); //Set BluetoothBee BaudRate to default baud rate 38400
blueToothSerial.print("\r\n+STWMOD=0\r\n"); //set the bluetooth work in slave mode
blueToothSerial.print("\r\n+STNA=SeeedBTSlave\r\n"); //set the bluetooth name as "SeeedBTSlave"
blueToothSerial.print("\r\n+STOAUT=1\r\n"); // Permit Paired device to connect me
blueToothSerial.print("\r\n+STAUTO=0\r\n"); // Auto-connection should be forbidden here
delay(2000); // This delay is required.
blueToothSerial.print("\r\n+INQ=1\r\n"); //make the slave bluetooth inquirable
Serial.println("The slave bluetooth is inquirable!");
delay(2000); // This delay is required.
blueToothSerial.flush();
}
[/color]

User avatar
Jacket Chen
Staff
Staff
Posts: 659
Joined: Thu Jun 21, 2012 4:25 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Seeeduino Shields
Location: China

Re: How do you communicate two SEEED BLUETOOTH?

Post by Jacket Chen » Fri May 17, 2013 9:39 am

hey , the demo of libraries from our wiki can't work well ? And i am not sure what's meaning of your code.
Love little, love long.

Post Reply