XBee Carrier - association LED flashes rapidly on battery

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
francgas
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Mon Jun 11, 2018 5:43 pm

XBee Carrier - association LED flashes rapidly on battery

Post by francgas » Mon Jun 11, 2018 7:07 pm

Good evening.

I purchased four Grove XBee Carrier boards to do some prototyping work and while the XBee (Digimesh 2.4 S2C) work fine from USB power it won't boot up under battery power (RX/TX lights solid red, ASSOC flashes rapidly). Interestingly powering it by USB then disconnecting USB allows the XBee to continue to operate on battery.

Has anyone seen this behaviour before?


Cheers,

Franc

PS - I wrote a full page analysis with measurements etc (took 2 hours) but the internet ate it. Arrrgh!

hong.jiang
Staff
Staff
Posts: 200
Joined: Tue Apr 17, 2018 11:03 am

Re: XBee Carrier - association LED flashes rapidly on battery

Post by hong.jiang » Thu Jun 14, 2018 11:03 am

Good morning:

When the XBEE boots up ,it needs more current than normal working condition.I'm afriad that your battery can not supply this system's boot up current(Digimesh 2.4 S2C also need more current when it goes to work).AS you found that( powering it by USB then disconnecting USB allows the XBee to continue to operate on battery) .When the system boots up instant by using battery ,the battery's voltage will decrease,and cause boot up fail.When the system has already boot up ,XBEE can operate on battery.

francgas
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Mon Jun 11, 2018 5:43 pm

Re: XBee Carrier - association LED flashes rapidly on battery

Post by francgas » Fri Jun 15, 2018 7:48 pm

Hi Hong.

Thanks for the response.

I measured the voltage on pin 1 of the XBee with an oscilloscope and it comes up at the same rate whether running off battery or USB. The voltage droops 1V for ~5uS at the battery when the power switch is turned, then returns to a steady level; there is no droop at pin 1 of the XBee Digimesh 2.4 S2C. If the battery can't provide the energy required I'd expect to see a longer or sustained droop.

The current draw for the XBee Digimesh 2.4 S2C is 33mA/28mA. This is similar to that 34.5mA/18.1m of the RFBee which, as stated on the XBee Carrier wiki is compatible with the XBee Carrier. It should work.

s.aldalahmeh
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sat Dec 22, 2018 3:54 pm

Re: XBee Carrier - association LED flashes rapidly on battery

Post by s.aldalahmeh » Mon Apr 29, 2019 8:33 pm

Dear All,

We are facing the same problem, your posts explained the reason behind this problem. Now is there a solution for it?

We tried batteries up to 6V batteries and other batteries with 3000 mAh batteries (twice the battery capacity that comes with the WSN kit) but with no luck.

We want a solution such that the Xbee boots from the battery with intervention since we want to use it in an outdoor application.

Thanks

Post Reply