Need help with Grove Serial Camera Code

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, salmanfarisvp, jeremy882, crail.lyu969

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Need help with Grove Serial Camera Code

Post by Anonymous » Fri May 03, 2019 7:51 pm

To whom it may concern,

I recently bought a Grove Serial Camera and tried this
Grove_Serial_Camera_Kit
https://github.com/Seeed-Studio/Grove_Serial_Camera_Kit>/
SerialCameral_DemoCode_CJ_
OV528/.
I am using it with the Seeed Studio, Base Shield V2 103030000 Base Shield
V2, Arduino.
and a *Wemos R1 D1.*

I am not having any success and really need help, as this is an important
project for university. Could you please provide me some advice. It will be
highly appreciated.

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Sun May 05, 2019 11:14 am

Hi 

Frederik, 

1. please take a picture about the hardware setup.

2. If you connect to hardware UART directly, you have to remove it when you download arduino program. 

3. You can connect to D2 port of the base shield and then run the https://github.com/Seeed-Studio/Grove_Serial_Camera_Kit/blob/master/SerialCameral_DemoCode_CJ_OV528_SoftSer/SerialCameral_DemoCode_CJ_OV528_SoftSer.ino , which use the software serial. 

4. What kinds error message do you have? 

Thanks

best rgds
Bill


Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

Post by Anonymous » Mon May 06, 2019 1:37 pm

Hi Bill,

Thank you so much, I managed to solve the problem. Now it is working
perfectly.

Post Reply