Grove - WS2813 RGB LED Strip and Seeeduino Lotus Cortex-M0+

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, salmanfarisvp, violet

Post Reply
alirazi
Pre-kindergarten
Pre-kindergarten
Posts: 16
Joined: Sat Aug 10, 2019 12:05 am

Grove - WS2813 RGB LED Strip and Seeeduino Lotus Cortex-M0+

Post by alirazi » Sat Aug 10, 2019 12:12 am

Is Grove - WS2813 RGB LED Strip Waterproof - 60 LED/m - 1m SKU 104020109 works with Seeeduino Lotus Cortex-M0+ SKU 102010228? It's IO Input Voltage is 3.3V

bill.yu
Junior-7
Junior-7
Posts: 735
Joined: Mon Apr 02, 2018 11:05 am

Re: Grove - WS2813 RGB LED Strip and Seeeduino Lotus Cortex-M0+

Post by bill.yu » Wed Aug 21, 2019 5:58 pm

Hi there~

The led strip max current is 3.6A per meter / 0.06A per LED. You can use the Seeeduino Lotus Cortex-M0+ to control the signal, GND. You can connect the external power supply(5V+GND) to led strip. thanks.

Post Reply