User interface

I have started making some changes to the code (in the original code the interface was hard to change as it was hard coded for each item which item came before / after it)

Changes from firmware v1.1:

  • Single-shot capture mode partially fixed (R0.3) [depending on the time base only part of the screen may show the signal]
  • grouped trigger functions
  • fixed bug that allowed trigger level to be continually moved down

code changes:

  • made it easier to change the menu order (to change the navigation order just change “enum menuItems” in Functions.h (to change the position on the screen change the coordinates in Functions.c)

Planned features:

  • AUTOSCALE

Compiling the code:

  • Download the official firmware and extract it - copy the folders DS0201_DFU, library, USBLib into a new folder and place DSO201_APP (from the attachment) in the folder.
  • Compile with IAR v5.4
  • DSO nano you will need to use the STMicroelectronics DfuSe programs (the output file is located in DS0201_APP\project\EWARM\Debug_FLASH\Exe) (you will need the hex file to a .dfu file)
  • Release 3 has some bugs in it and I don’t recommend using this version for normal use.

  • This version of the software is based on v1.1 of the original software. Due to the limitations of this loading / saving to the micro SD card might not work.
    DSO201.R0.3.dfu.zip (20.2 KB)
    DSO R0.3.zip (64.9 KB)
    DS0201_APP_r0.2.zip (131 KB)