Page 1 of 1

Maix-Bit V2.0 programming problem

Posted: Wed Jul 10, 2019 7:24 am
by bruceh
I have Maix-Bit V2.0 and cannot program it from Arduino using Maxduino(K210) Version 0.3.9 on Mac Mojave 10.14.5, arduino 1.8.8
I can program a Maix-Bit V1.09 successfully.
Version 2.0 error:
...
Sketch uses 322706 bytes (3%) of program storage space. Maximum is 8388608 bytes.
[INFO] ANSI colors not used
[INFO] COM Port Selected Manually: /dev/cu.usbserial-00001014B
[INFO] Default baudrate is 115200 , later it may be changed to the value you set.
[INFO] Trying to Enter the ISP Mode...
...............
Greeting fail, check serial port ([ERROR] No vaild Kendryte K210 found in Auto Detect, Check Your Connection or Specify One by`-p /dev/ttyUSB0` )
Greeting fail, check serial port ([ERROR] No vaild Kendryte K210 found in Auto Detect, Check Your Connection or Specify One by`-p /dev/ttyUSB0` )

Please help. I just purchased 50 of these boards. Neither port /dev/cu.usbserial-00001014A or /dev/cu.usbserial-00001014B work.

Re: Maix-Bit V2.0 programming problem

Posted: Wed Jul 10, 2019 10:22 am
by bill.yu
Hi there~,

Please check if the usb cable is 4 wires for data transfer. thanks.

Re: Maix-Bit V2.0 programming problem

Posted: Wed Jul 10, 2019 10:48 am
by bruceh
Yes. The same cable and software programed a Maix-Bit V1.09 successfully.
Perhaps the k-flash programmer software didn't get updated correctly in Maxduino(K210) Version 0.3.9 to support the Maix-Bit V2.0?

Re: Maix-Bit V2.0 programming problem

Posted: Wed Jul 10, 2019 10:59 am
by bill.yu
Hi there~

I am checking with the designer and will keep you posted here. thanks.

Re: Maix-Bit V2.0 programming problem

Posted: Thu Jul 11, 2019 3:51 pm
by bill.yu
Hi there~

You can select maixduino board to download for Maix bit v2.0 as temporary solution. we will add MAIX Bit V2.0 support this week. thanks.

Re: Maix-Bit V2.0 programming problem

Posted: Fri Jul 12, 2019 2:24 am
by bruceh
That works, thank you!

Re: Maix-Bit V2.0 programming problem

Posted: Thu Jul 18, 2019 6:43 am
by bruceh
Do you have an estimated delivery time for Maxduino(K210) Version to support the Maix-Bit V2.0?

Re: Maix-Bit V2.0 programming problem

Posted: Tue Jul 30, 2019 10:37 am
by bill.yu
Hi there~

Please update maixduino to rev 0.3.10. It can solve the issue. thanks.