XIAO SWD connector

Hi,

I have just received my XIAO.
What I found awesome is that there are SWD I/O are exposed, but on testing pads.
I would like to know if you could provide an Eagle library with SWD pad footprint or any simple solution which could cleanly expose those pin to a standard SWD 10 pins connector (I don’t wan’t to solder crappy wires on the pads.), because the SWD pads are not aligned on a 2.54mm grid.

I could eventually make a custom carrier board. Which connector do you use on Seeeduino XIAO Expansion board (spring contact)?

Thanks by advance,

Thomas

It seems the Seeeduino XIAO Expansion board already features pogo-pins for debugging.

Please refer to

Glad to know that you find the exposed SWD I/0 design useful for you.
The spring contact we use in SeeeduinoXIAO Expansion Board is customized, and purchased from designated contributor at a minimum order quantity. It well fits pin header of both 6mm and 5mm height. If you think SWD function is necessary for you, it would be highly recommended that you get one. :slight_smile:

Thanks for your anwser.

I have already seen the Expansion board, but not available yet. Also I would like to design my own expansion board, so I’ll need dimensions or any informations to be able to connect the SWD pins.

Thanks for your anwser. Could you please provide the cotations to be able to well position the pogo pins ?

I think it would be great to have a XIAO footprint with those pins exposed in your Eagle library :slight_smile:

Hi, detailed learn and documents you required could be found under this page: https://www.seeedstudio.com/Seeeduino-XIAO-Arduino-Microcontroller-SAMD21-Cortex-M0+-p-4426.html

Ok, thanks, I guess I can make cotations from the brd file.

PS : it looks like this is not the latest design which is available on the link you gave (missing reset and gnd test pads)

check this: http://files.seeedstudio.com/wiki/Seeeduino-XIAO/HDK/v1.0/102010328_Seeeduino_XIAO_Dimension_bottom.dxf

Thanks a lot. Thanks to Autodesk Viewer (https://viewer.autodesk.com) I can check the quotations from the file you reffer to. Really appreciate

Is there an off the shelf pogo pair to order here for this placement?

You can order similar things like the Mill-Max 827-22-004-10-001101. But stock and prices are all over the place. Also, it’s still tough to get the right height.

Adafruit 5382 is an inexpensive 2 x 3 pogo. You can carefully push out two pins, cut through the holes with dykes, then dress with a file.

The layout of the SWD is 0.1” but on an 0.05” grid so it does not play nicely with perfboards. Also, to mate with 8.5 mm female header supported boards it needs about 2 mm spacer. I printed a little U-shaped thing that fits tightly between the female headers. The centering in that direction is perfect. The positioning in the other direction can be adjusted and then a drop of glue does it.

I had some very nice photos but it won’t let me. In any case, it worked out great.

Hi there,

Spam protection thingy, maybe a couple more reply’s will get enough creds to post the pics, This area is probably the least addressed from maker or manufacture it get’s the "Rodney Dangerfield " , NO -Respect :grin:

On my 3D printed sockets, I had similar but finally got it after a few prints

HTH
GL :slight_smile: PJ :v:

But that’s going the reverse direction. What’s the use case for that?

Hi there,

SO the use case is everywhere and no soldering :grin:
here is the correct perspective.

Started out as a ZIF socket idea, then wanted the SWD features, the battery Pads and so..




Push and Pressure fit






HTH
GL :slight_smile: PJ :v:

Links to ALL the 3D printed stuff on my Thingiverse :+1: