XIAO Sense - charging a LiPo battery

There are several codes posted already. This is from one of those. I just added USB detection to it. Extracted from long code, you may need to tweak it… Careful with fixing long comment lines wrap around, if you copy it or will not compile!



//only for version 1.0 of XIAO BLE SENSE
//main codes are from posts at the XIAO forum
//added USB detection codes


#include <Arduino.h>

#define BAT_READ 14            // P0_14 = 14  Reads battery voltage from divider on signal board. (PIN_VBAT is reading voltage divider on XIAO and is program pin 32 / or P0.31)
#define CHARGE_LED 23          // P0_17 = 17  D23   YELLOW CHARGE LED
#define HICHG 22               // P0_13 = 13  D22   Charge-select pin for Lipo for 100 mA instead of default 50mA charge

const double vRef = 3.3; // Assumes 3.3V regulator output is ADC reference voltage
const unsigned int numReadings = 1024; // 10-bit ADC readings 0-1023, so the factor is 1024

volatile int BAT_CHRG; //is the battery connected and charging?   5V connected/charging = 0; disconnected = 1


void setup() {
  // put your setup code here, to run once:

  Serial.begin(115200);
  delay(100);

  pinMode (CHARGE_LED, INPUT);  //sets to detetct if charge LED is on or off to see if USB is plugged in
  pinMode (HICHG, OUTPUT);  digitalWrite(HICHG, LOW);  //100 mA charging current if set to LOW and 50mA (actually about 20mA) if set to HIGH
  pinMode(BAT_READ, OUTPUT);  digitalWrite(BAT_READ, LOW);// This is pin P0_14 = 14 and by pullling low to GND it provices path to read on pin 32 (P0,31) PIN_VBAT the voltage from divider on XIAO board

  /*
    printf("\nBattery Test compiled by davekw7x on %s at %s\n",   __DATE__, __TIME__);
    printf("Note: PIN_VBAT = %u\n\n", PIN_VBAT);
  */
}

///////////////////////////////////////////////////////////////////////READ LIPO BATTERY////////////////////////////////////////////////////////////////
void readBAT()  {
  unsigned int adcCount = analogRead(PIN_VBAT);//  PIN_VBAT is reading voltage divider on XIAO and is program pin 32 or P0.31??
  double adcVoltage = (adcCount * vRef) / numReadings;
  double vBat = adcVoltage * 1675.0 / 510.0; // Voltage divider from Vbat to ADC  // was set at 1510.0...set your own value to calibrate to actual voltage reading by your voltmeeter
  printf("adcCount = %3u = 0x%03X, adcVoltage = %.3fV, vBat = %.3f\n", adcCount, adcCount, adcVoltage, vBat);
  delay(10);

}
///////////////////////////////////////////////////////////////////////END OF READ LIPO BATTERY////////////////////////////////////////////////////////////////


void loop() {
  // put your main code here, to run repeatedly:

 
  BAT_CHRG = digitalRead(CHARGE_LED);  //

  if (BAT_CHRG == 1)  {  //if USB/charger IS NOT plugged in

    // Serial.print("  Battery Charge status =  "); Serial.println(BAT_CHRG);
    Serial.println(" USB -IS NOT- plugged in ");     //do whatever you want here once USB is detected, in order to make sure user knows that battery-read values are now USB-generate
    }

  if (BAT_CHRG == 0) {   ////if USB/charger IS plugged in
     // Serial.print("  Battery Charge status =  "); Serial.println(BAT_CHRG);
     Serial.println(" USB -IS- plugged in ");     //do whatever you want here once USB is detected, in order to make sure user knows that battery-read values are now USB-generated
  }
  
  readBAT();   // loops back to lipo BAT read routine
  
  delay(5000);//delays 5 sec betwen battery readings


}  //END OF LOOP

1 Like