Hi there,
Well I got WHite SO Bright you need to wear SHADES… ![]()
Try this does it run ?
#include <Adafruit_NeoPixel.h>
#define LED_PIN 12 // GPIO12 (D12) controls the onboard WS2812
#define NUM_LEDS 1
Adafruit_NeoPixel led(NUM_LEDS, LED_PIN, NEO_GRB + NEO_KHZ800);
void setup() {
led.begin(); // Initialize the LED strip
led.show(); // Turn off all LEDs initially
}
void loop() {
// Red
led.setPixelColor(0, led.Color(255, 0, 0));
led.show();
delay(1000);
// Green
led.setPixelColor(0, led.Color(0, 255, 0));
led.show();
delay(1000);
// Blue
led.setPixelColor(0, led.Color(0, 0, 255));
led.show();
delay(1000);
// White
led.setPixelColor(0, led.Color(255, 255, 255));
led.show();
delay(1000);
}
LMK
GL
PJ ![]()
note: and yes, the onboard WS2812B LED is still controlled via GPIO 12, just like on the standard RP2040 version. the Seeed XIAO RP2040 has a built-in WS2812B RGB LED (usually on pin D12 / GPIO 12), and you can control it using the Adafruit_NeoPixel library.
Chart on WiKi:
2340 1 user LED(3 colors), 1 power LED, 1 RGB LED
2350 1 user LED, 1 charge LED(Battery Charging Indicator),1 RGB LED
![]()