🧐 Xiao nRF54L15 with Round Display... mind the KE switch!

So Yea, It’s a GO with the round display , build on 3.1.1
LVGL example…
NO MCUBOOT ,just does it work test, filmed on a Potato :potato: :film_projector:

GL :slight_smile: PJ :v:

1 Like

Hi there,

SO watch face time… Let’s start there. :grin:
I have enclosed the project folder, You know what to do. :+1:
if not read the read me. (if need be I can do a walkthrough of the process, it’s easy once you get it down.)

Watchface-ZIP

so the Zip is there. the project folder, mind the readme.text

HTH
GL :slight_smile: PJ :v:

2 Likes

I think that was added in later versions too… so if you have the ulgtra rare prototype version…

Hi there,

Yea, I think I have one of each, But this is using LVGL, I like the TFT_eSPI lib better. but it’s a start :+1: Glad it works is all here, before some DH starts yakin. :grin:
It’s a great display ,would be nice to have a bare bonzes model Display and Touch only. :crossed_fingers:
:mega: :bust_in_silhouette:

THIN

would be REAL nice :face_with_hand_over_mouth:

GL :slight_smile: PJ :v:

Great idea. I really like it.
When it’s up and running, it would be good to add it to the wiki: