Xiao nrf52840 Surface mount

Hello,

I’m wondering if anyone has any experience with surface mounting the XIAO nrf52840 to a PCB. I’m trying to use it for a wearable and so avoiding the thickness/height of headers would be good.

I’d also like to use the VBATT pads on the underside connected to the battery which will be VDD. Doing it this way because the NRF52840 can’t output enough current for what I have on the rest of the PCB so I was going to use the battery as Vdd and Gnd and connect these to the Vbatt pins so I can deliver appreciable current (~0.5A) from the battery but still make use of the charging circuitry of the XIAO nrf52840.

I’ve seen there’s a surface mount footprint for the board on the getting started page, I just haven’t seen anyone use it as surface mount so was wondering why.

Any info/ideas would be appreciated!

Check this out for some ideas:

https://fabacademy.org/2024/labs/charlotte/students/richard-shan/lessons/week4/rp2040/

Hi there,

Oh’ you haven’t lived until you SMD solder the Xiao… :grin:
Totally fine, Keep READING buddy :nerd_face:

here is some fresh ones, those are some older Pics.
and don’t do like the first one, from a user on here, was using a potato to solder.

The 3 channel EMG board it the grove EMG Board x3 (i squeezed it on there 45mm roundy round, the concept for adding the xiao directly on SMD pin Header receptacles. :+1:

The Evolution is to OVAL the Battery Pad Through holes and plated through also. a little bigger is better but not Wider the the Xiao’s PAD
AMA

HTH
GL :slight_smile: PJ

Solder “Paste” is your friend. :ok_hand:





Hi,

That’s massively helpful thank you

So it is possible. You say “The Evolution is to OVAL the Battery Pad Through holes and plated through also. a little bigger is better but not Wider the the Xiao’s PAD” but I’m not too sure what is meant. Is OVAL a technical term or oval as in an ellipse? Also not sure about the “battery pad through holes” they are just pads no? Are you suggesting via in pad for them and if so can I not just route them on the same layer?

I was also wondering if there are any requirements for below the antenna. Should I have this as a “keep out” on the below board?

Thanks again!

Hi there,

So , Don’t overthink it. Oval or “Elongated” then would probably define better. Just be sure you go heavier on the Plated through parts.
NO, NO,NO… keep out of that Zone or you won’t get any distance that’s the important part to have good BLE transmission.

Look at this;

the C3 cap in the pic is the closest you’ll want to go. :+1:
This 2nd one had a display and when the display cable was connected the BLE was less distance.

HTH
GL :slight_smile: PJ :v:

So I found these later pics of the Current tech delivering 100% success :+1:

Paste the edges of the ovals on the top side, Paste the the PADS on the bottom of the Xiao. Clamp lightly…, :pinching_hand: flip it over and solder the bottom. after the paste melts feed the solder roll into the holes (slowly, fill it.)

You can solder only the pins you plan to use or solder them all.
YMMV , and consult your specific technical reference guides.

HTH
GL :slight_smile: PJ :v:

Thanks again! Is that necessary if you have a hotplate or oven to solder it with, or is this just for trying to do it by hand?

Hi there,

So mostly for by hand, but you’ll need to apply paste to both the stencil for the board and on the Xiao’s Batt Pads Only… YMMV but I get :100: percent success when applying this tech. :crossed_fingers:

HTH
GL :slight_smile: PJ :v:

Are you using a really fine soldering tip or using solder paste?

I think, are you state, my ovals are too big (nor fully aligned either), but I feel this should work. However, it’s almost never does.

I’m wondering if a finer soldering iron would help me make the connection with a small blob of solder.

Also wondering if I could apply some solder paste and put it on my mini hot plate.

Thoughts appreciated!

Hi there,

Yes , Solder paste is the way to go. Looks pretty good a TAD on the big side… but it should work. I use the tiny tip to touch the pad from the bottom of the hole. then add roll solder but I paste and flux EVERYTHING a LOT first :grin: It works 100%

Stay at it you’ll get there. Looks GOOD! :+1:

HTH
GL :slight_smile: PJ :v:

I would have loved to see these designs six months ago. Good stuff. I just made a large cutout on my own board design so that the pads on the bottom of the xiao board were accessible.

Hi there,

And LOL, most definitely Welcome here… :grin:

When You know, You know… NOW , YOU know :+1:

Good stuff indeed.

GL :slight_smile: PJ :v:

Hi, late to the party but I have a question regarding the antenna keep out zone. Is it okay to have grounded zones below the XIAO on both sides of the PCB? Does the Bluetooth still work then?

Or what do I have to keep in mind while finding a way to place the antenna?

Hi there,

So, on m/y own PCB’s I found the area immediately behind the ceramic wants no traces , ground plane was Aok, here is an early PCB pic. :+1: One of many
:grin:


HTH
GL :slight_smile: PJ :v:

The datasheet (and basic RF knowledge) recommends keeping the ground planes (and traces and components) away from the chip antenna, especially if placing a surface mount XIAO part.

From PCBSync…

The design above shows a ground plane under the chip antenna. RF will be affected.

Some exceptions are… if using a L-shaped single wire antenna above the ground plane (freeform inverted-L) or vertical radiating antenna.